TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » OMAP™ Processors » OMAP-L13x, AM1x and C674x Processors Forum » OMAP-L138 Booting from SPI ATMEL
Share
OMAP™ Processors
  • Forums
  • Announcements
Options
  • Subscribe via RSS
Resources
  • OMAP-L1x DSP+ARM9™-based Processors Product Folder
  • OMAP3525/30 DSP+ARM Cortex™-A8-based SOCs Product Folder

  • Top OMAPL Wiki Links
  • OMAPL3x Schematic Review Checklist
  • OMAPL13x Boot resources

  • OMAPL Document Resources
  • OMAPL137 Technical reference manual
  • OMAPL138 Technical reference manual
  • OMAPL Boot loader App Notes
  • OMAP-L138 Booting from SPI ATMEL

    OMAP-L138 Booting from SPI ATMEL

    This question is answered
    raneliya
    Posted by raneliya
    on May 26 2011 08:08 AM
    Genius5270 points
    Hello, I am using a custom board with OMAP-L138 And SPI flash of ATMEL AT45DB321D. I flashed the SPI using CCS4 with spi-flash-writer( I had to add support for ATMEL since the spi-flash-writer 3.20.00.XX does not include support for atmel). Anyway, I get that the application succeed in reading with the text "File Match". I flashed first arm-spi-ais.bin - "armais" file, but after reseting in mode booting from SPI1 flash (0x0C in boot configuration register), I get no printing at all in UART. I tried to change page size from 528 to 512, and flashed again the armais file but still nothing... Can it be that OMAP cannot boot from ATMEL, or is there anything else wrong in my configuration ? I thank you for your help, Ran Shalit
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    All Replies
    • 1258021
      Posted by 1258021
      on May 26 2011 22:38 PM
      Genius4330 points

      Hi Ran Shalit,

      I hope you have interfaced the SPI Flash according to the user guide which is avaialbale at the following URL

      http://focus.ti.com/dsp/docs/litabsmultiplefilelist.tsp?sectionId=3&tabId=409&literatureNumber=sprab41c&docCategoryId=1&familyId=1621

      Looks the constraints specified in above user guide are met by your device,  24-Bit addr and support a read command value of (0x03).

      I hope you are not using any chip select other than CS0.

      Regards,

      GSR

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Daniel Allred
      Posted by Daniel Allred
      on May 26 2011 23:34 PM
      Genius15085 points

      I agree with 1258021(aka GSR). The read command (0x03) is supported by the device as "Continuous Array Read (Low Frequency Mode)".  The address is 22 bits in 512 byte mode (which you will have to use, as the addressing scheme in 528 byte mode is not compatible).

      Since this appears to be a custom board, you may also need to change some aspects of the UBL. In particular, I thinking that if you have an oscillator or crystal that works at a different frequency, the UBL included will not setup the UART as needed for 1152008n1 operation.

      Finally, if you have the JTAG connection, you can try using the debug GEL files to see if you can get more info about what is going on during a failed boot.

      Regards, Daniel

      ----------------------------------------------------------------------------------------------------------
      Please click the
      Verify Answer button on this post if it answers your question.
      ----------------------------------------------------------------------------------------------------------

       

      SPI boot flash SPI flash
      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • raneliya
      Posted by raneliya
      on May 27 2011 09:31 AM
      Genius5270 points
      atmel_datasheet.pdf

      Hi Dandiel & GSR,

      Thank you for your ideas.

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • raneliya
      Posted by raneliya
      on May 27 2011 09:44 AM
      Genius5270 points

      Hi Daniel & GSR,

      Thank you for your ideas.

      • the continous read command (0x3) is supported by AT45DB321D.
      • I see that for 528 page it uses 23 bits, and for 512 page it uses 22 bits:

       "Buffer addressing for the DataFlash standard page size (528 bytes) is referenced in the
      datasheet using the terminology BFA9 - BFA0 to denote the 10 address bits required to designate
      a byte address within a buffer. Main memory addressing is referenced using the
      terminology PA12 - PA0 and BA9 - BA0, where PA12 - PA0 denotes the 13 address bits
      required to designate a page address and BA9 - BA0 denotes the 10 address bits required to
      designate a byte address within the page.
      For “Power of 2” binary page size (512 bytes) the Buffer addressing is referenced in the
      datasheet using the conventional terminology BFA8 - BFA0 to denote the 9 address bits
      required to designate a byte address within a buffer. Main memory addressing is referenced
      using the terminology A21 - A0, where A21 - A9 denotes the 13 address bits required to designate
      a page address and A8 - A0 denotes the 9 address bits required to designate a byte
      address within a page.

      On my previous trials, I configured the flash for 512 page size, and flash the UBL again,
      but still I did not see any characters in the UART when booting from SPI Flash.

      • what did you mean about changing some aspects of the UBL ? does the UBL fits itslef only to the OMAP-L138 EVM? how do I change the UBL and what should I change in it?
      • I saw in the CC studio that the boot configuration register is set for booting from spi flash (0xc) , is there something else maybe I should watch in particular on the failed boot.

      I have attached the atmel datasheet in the previous post (sorry for sending the previous message not complete).

      >Interesting thing to Note here is that the flash program read phase (after the writing) verifies that writing is successful , so does not that mean that the flashing was OK ?

      Thank you !!!

      Ran

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • raneliya
      Posted by raneliya
      on May 27 2011 09:48 AM
      Genius5270 points

      Hello GSR,

      Thank you for your support,
      I see that the atmel uses 22 bit address for 512 page, and 23-bit for 528 address, Does it mean that there is problem here with the 24-bit addressing constrain ?
      I have attched the datasheet in the previous message.

      >Interesting thing to Note here is that the flash program read phase (after the writing) verifies that writing is successful , so does not that mean that the flashing was OK ?

      Thank you !!!

      Ran

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Daniel Allred
      Posted by Daniel Allred
      on May 27 2011 10:22 AM
      Genius15085 points

      ran shalit

      Hello GSR,

      Thank you for your support,
      I see that the atmel uses 22 bit address for 512 page, and 23-bit for 528 address, Does it mean that there is problem here with the 24-bit addressing constrain ?
      I have attched the datasheet in the previous message.

      The ROM boot loader will linearly increment the address (unless you turn on sequential read, in which case a single read command and address is sent and then the memory device is just expected to spit out data while incrementing on its own). In any case, the ROM boot loader does not know anything about pages and splitting the address bits between pages and blocks, so the 528 byte mode won't work. It may work in sequential read mode because all of the upper address bits during the reads from the start of the memory will be zero, but the device data sheet can specify what happens in that case.

      Regards, Daniel

      ----------------------------------------------------------------------------------------------------------
      Please click the
      Verify Answer button on this post if it answers your question.
      ----------------------------------------------------------------------------------------------------------

       

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • raneliya
      Posted by raneliya
      on May 27 2011 11:23 AM
      Genius5270 points

      Hi Daniel,

      So does it mean that Although it is 22 bit address for 512 page, and not 24 bits, I can still use it?
      I see that the spi-flash-writer, verifies that file match, which means (if I'm correct) that the UBL is flashed correctly in the SPI flash.  
      But after setting 512 page configuration, and getting "file match" for the UBL flash, there is still nothing in the UART.
      Does it mean that the UBL does not fit my configuration. What steps you suggest me to take ?

      Regards,

      Ran

      spi-flash-writer/main.c

      .....

        while(!feof(fPtr))
          {
        unsigned int nbytes;

           if(!feof(fPtr)) {
         nbytes = fread(tx, 1, page_size, fPtr);
        }  
        tx[nbytes] = '\0';

        flash->read (flash, i * page_size, page_size, (Uint8 *)rx);
              rx[nbytes] = '\0';
        if(strcmp((const char *)rx,(const char *)tx)!= 0) {
         printf("Files did not match @ %d\n", ftell(fPtr));
         goto finish;
        }
        i++;
          }

       printf("Files matched \n");

       

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Daniel Allred
      Posted by Daniel Allred
      on May 27 2011 11:34 AM
      Genius15085 points

      The ROM will always send out 24 address bits.  This matches with what this Atmel device expects, so there is no issue (only 22 of the bits will mean anything to the Atmel device and unless the ROM tries to read past the end of the flash, those upper two bits will always be zero anyways).

      Please use the debug gel file I mentioned earlier to try and get the status of the ROM boot process.

      Also, have you followed the directions in the section 13 of the datasheet to permanently configure the device for 512 byte (power of two) page size? Is that what you mean when you say "setting 512 page configuration"?

      Regards, Daniel

      ----------------------------------------------------------------------------------------------------------
      Please click the
      Verify Answer button on this post if it answers your question.
      ----------------------------------------------------------------------------------------------------------

       

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • raneliya
      Posted by raneliya
      on May 27 2011 11:42 AM
      Genius5270 points

      Yes, I've configured the device to permanently use 512 byte page (and reset the system afterwards), and the flashed the UBL again (I was able to see that the ATMEL configuration was changed to 512 bytes page, becuase it prints the page size in the probing function).

      I use the LogicPD Gel file (same as in the EVM), meanwhile without any changes. What did you mean about the boot process state ? should I see where the PC is and try to understand what functions were fetched from the SPI memory?

      Do I need to create new UBL file before flashing it into the SPI flash or does the UBL file should match any configuration?

      Regards,

      Ran

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Daniel Allred
      Posted by Daniel Allred
      on May 27 2011 11:50 AM
      Genius15085 points

      ran shalit

      I use the LogicPD Gel file (same as in the EVM), meanwhile without any changes. What did you mean about the boot process state ? should I see where the PC is and try to understand what functions were fetched from the SPI memory?

      See the link I mentioned earlier: http://processors.wiki.ti.com/index.php/OMAP-L1x_Debug_Gel_Files

      If the boot fails, you can use this file to get some info from the device about what happened.

      Regards, Daniel

       

      ----------------------------------------------------------------------------------------------------------
      Please click the
      Verify Answer button on this post if it answers your question.
      ----------------------------------------------------------------------------------------------------------

       

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • raneliya
      Posted by raneliya
      on May 29 2011 02:11 AM
      Genius5270 points

      Hi Daniel,

      I have continued the diagnostics today, I see some interesting things:

      1. I am trying to burn only boot-strap meanwhile (without u-boot). As I undestand it should give me some printing in UART anyway, even if u-boot is not flashed. Also if I'm currect I can flash the boot-strap also in other boot modes (not only emulator) since the emulator will always take control on the board. I hope it is OK to work this way.

      2. I see that flashing the SPI flash image/boot-strap/arm-spi-ais.bin does not give me any printings in UART. the disagnotics are at the end of this message. I then tried to flash the bin image of the "flash and boot utils" called ubl_OMAPL138_SPI_MEM.bin. I was surprised to see that the UBL now starts and gives printings in UART , although I get "no magic number is found" in the printings (?). the diagnotics here are the same( except to PC register) for both case.

      3. Same thing as 2 happend when I tried to flash the Nand in my board: flashing the bin from  image/boot-strap/arm-nand-ais.bin gives nothing, but flashing the ubl_OMAPL138_NAND.bin gives printing (UBL works). the diagnotics here are the same( except to PC register) for both cases.

      Any advice is appreciated , Thank you for the help !

      Ran

       

      ARM9_0: Output:  Target Connected.
      ARM9_0: Output:  ---------------------------------------------
      ARM9_0: Output:  Memory Map Cleared.
      ARM9_0: Output:  ---------------------------------------------
      ARM9_0: Output:  Memory Map Setup Complete.
      ARM9_0: Output:  ---------------------------------------------
      ARM9_0: Output:  KICK Unlocked.
      ARM9_0: Output:  ---------------------------------------------
      ARM9_0: Output:  PSC Enable Complete.
      ARM9_0: Output:  ---------------------------------------------
      ARM9_0: Output:  PLL0 init done for Core:300MHz, EMIFA:25MHz
      ARM9_0: Output:  mDDR initialization is in progress....
      ARM9_0: Output:  PLL1 init done for DDR:150MHz
      ARM9_0: Output:  Using mDDR settings
      ARM9_0: Output:  mDDR init for 150 MHz is done
      ARM9_0: Output:  ---------------------------------------------
      ARM9_0: Output:  DSP Wake Complete.
      ARM9_0: Output:  ---------------------------------------------
      ARM9_0: GEL Output:
      ---------------------------------------------
      ARM9_0: GEL Output: |             Device Information            |
      ARM9_0: GEL Output: ---------------------------------------------
      ARM9_0: GEL Output: DEV_INFO_00 = 0x1B7D102F
      ARM9_0: GEL Output: DEV_INFO_01 = 0x00000000
      ARM9_0: GEL Output: DEV_INFO_02 = 0x0000000C
      ARM9_0: GEL Output: DEV_INFO_03 = 0x00000032
      ARM9_0: GEL Output: DEV_INFO_04 = 0x00000000
      ARM9_0: GEL Output: DEV_INFO_05 = 0x000003E0
      ARM9_0: GEL Output: DEV_INFO_06 = 0x00000080
      ARM9_0: GEL Output: DEV_INFO_07-DEV_INFO_08-DEV_INFO_09-DEV_INFO_10-DEV_INFO_11-DEV_INFO_12 = 0-0-5621784-22-46-19
      ARM9_0: GEL Output: DEV_INFO_13,DEV_INFO_14,DEV_INFO_15,DEV_INFO_16 = 2,0,0,11272
      ARM9_0: GEL Output: -----
      ARM9_0: GEL Output: DEV_INFO_17 = 0x00030003
      ARM9_0: GEL Output: DEV_INFO_18 = 0x00000000
      ARM9_0: GEL Output: DEV_INFO_19 =ARM9_0: GEL Output: 0ARM9_0: GEL Output: 0ARM9_0: GEL Output: 0ARM9_0: GEL Output: 0ARM9_0: GEL Output: 0ARM9_0: GEL Output:
      ARM9_0: GEL Output: -----
      ARM9_0: GEL Output: DEV_INFO_20 = 0x30303864
      ARM9_0: GEL Output: DEV_INFO_21 = 0x3630306B
      ARM9_0: GEL Output: DEV_INFO_22 = 0x30303864
      ARM9_0: GEL Output: DEV_INFO_23 = 0x3630306B
      ARM9_0: GEL Output: -----
      ARM9_0: GEL Output: DEV_INFO_24 = 0x1601302E
      ARM9_0: GEL Output: DEV_INFO_25 = 0x0055C818
      ARM9_0: GEL Output: DEV_INFO_06 = 0x00000080
      ARM9_0: GEL Output: DEV_INFO_26 = 0x58100002
      ARM9_0: GEL Output:

      ARM9_0: GEL Output: ---------------------------------------------
      ARM9_0: GEL Output: |               BOOTROM Info                |
      ARM9_0: GEL Output: ---------------------------------------------
      ARM9_0: GEL Output: ROM ID: d800k006
      ARM9_0: GEL Output: Silicon Revision 2.0
      ARM9_0: GEL Output: Boot Mode: SPI1 Flash
      ARM9_0: GEL Output:
      ROM Status Code: 0x00000000
      Description:ARM9_0: GEL Output: No error
      ARM9_0: GEL Output:
      Program Counter (PC) = 0x019482B8
      ARM9_0: GEL Output:
      ARM9_0: GEL Output: ---------------------------------------------
      ARM9_0: GEL Output: |              Clock Information             |
      ARM9_0: GEL Output: ---------------------------------------------
      ARM9_0: GEL Output:
      ARM9_0: GEL Output: PLLs configured to utilize crystal.
      ARM9_0: GEL Output: ASYNC3 = PLL0_SYSCLK2
      ARM9_0: GEL Output:
      ARM9_0: GEL Output: NOTE:  All clock frequencies in following PLL sections are based
      ARM9_0: GEL Output: off OSCIN = 24 MHz.  If that value does not match your hardware
      ARM9_0: GEL Output: you should change the #define in the top of the gel file, save it,
      ARM9_0: GEL Output: and then reload.
      ARM9_0: GEL Output:
      ARM9_0: GEL Output: ---------------------------------------------
      ARM9_0: GEL Output: |              PLL0 Information             |
      ARM9_0: GEL Output: ---------------------------------------------
      ARM9_0: GEL Output:
      ARM9_0: GEL Output: PLL0_SYSCLK1 = 300 MHz
      ARM9_0: GEL Output: PLL0_SYSCLK2 = 150 MHz
      ARM9_0: GEL Output: PLL0_SYSCLK3 = 25 MHz
      ARM9_0: GEL Output: PLL0_SYSCLK4 = 75 MHz
      ARM9_0: GEL Output: PLL0_SYSCLK5 = 300 MHz
      ARM9_0: GEL Output: PLL0_SYSCLK6 = 300 MHz
      ARM9_0: GEL Output: PLL0_SYSCLK7 = 50 MHz
      ARM9_0: GEL Output:
      ARM9_0: GEL Output: ---------------------------------------------
      ARM9_0: GEL Output: |              PLL1 Information             |
      ARM9_0: GEL Output: ---------------------------------------------
      ARM9_0: GEL Output:
      ARM9_0: GEL Output: PLL1_SYSCLK1 = 300 MHz
      ARM9_0: GEL Output: PLL1_SYSCLK2 = 150 MHz
      ARM9_0: GEL Output: PLL1_SYSCLK3 = 300 MHz
      ARM9_0: GEL Output:
      ARM9_0: GEL Output: ---------------------------------------------
      ARM9_0: GEL Output: |              PSC0 Information             |
      ARM9_0: GEL Output: ---------------------------------------------
      ARM9_0: GEL Output:
      ARM9_0: GEL Output: State Decoder:
      ARM9_0: GEL Output:  0 = SwRstDisable (reset asserted, clock off)
      ARM9_0: GEL Output:  1 = SyncReset (reset assered, clock on)
      ARM9_0: GEL Output:  2 = Disable (reset de-asserted, clock off)
      ARM9_0: GEL Output:  3 = Enable (reset de-asserted, clock on)
      ARM9_0: GEL Output: >3 = Transition in progress
      ARM9_0: GEL Output:
      ARM9_0: GEL Output: Module 0: EDMA3CC (0)        STATE = 3
      ARM9_0: GEL Output: Module 1: EDMA3 TC0          STATE = 3
      ARM9_0: GEL Output: Module 2: EDMA3 TC1          STATE = 3
      ARM9_0: GEL Output: Module 3: EMIFA (BR7)        STATE = 3
      ARM9_0: GEL Output: Module 4: SPI 0              STATE = 3
      ARM9_0: GEL Output: Module 5: MMC/SD 0           STATE = 3
      ARM9_0: GEL Output: Module 6: AINTC              STATE = 3
      ARM9_0: GEL Output: Module 7: ARM RAM/ROM        STATE = 3
      ARM9_0: GEL Output: Module 9: UART 0             STATE = 3
      ARM9_0: GEL Output: Module 10: SCR 0 (BR0/1/2/8)  STATE = 3
      ARM9_0: GEL Output: Module 11: SCR 1 (BR4)        STATE = 3
      ARM9_0: GEL Output: Module 12: SCR 2 (BR3/5/6)    STATE = 3
      ARM9_0: GEL Output: Module 13: PRUSS              STATE = 0
      ARM9_0: GEL Output: Module 14: ARM                STATE = 3
      ARM9_0: GEL Output: Module 15: DSP                STATE = 3
      ARM9_0: GEL Output:
      ARM9_0: GEL Output: ---------------------------------------------
      ARM9_0: GEL Output: |              PSC1 Information             |
      ARM9_0: GEL Output: ---------------------------------------------
      ARM9_0: GEL Output:
      ARM9_0: GEL Output: State Decoder:
      ARM9_0: GEL Output:  0 = SwRstDisable (reset asserted, clock off)
      ARM9_0: GEL Output:  1 = SyncReset (reset assered, clock on)
      ARM9_0: GEL Output:  2 = Disable (reset de-asserted, clock off)
      ARM9_0: GEL Output:  3 = Enable (reset de-asserted, clock on)
      ARM9_0: GEL Output: >3 = Transition in progress
      ARM9_0: GEL Output:
      ARM9_0: GEL Output: Module 0: EDMA3CC (1)        STATE = 3
      ARM9_0: GEL Output: Module 1: USB0 (2.0)         STATE = 3
      ARM9_0: GEL Output: Module 2: USB1 (1.1)         STATE = 3
      ARM9_0: GEL Output: Module 3: GPIO               STATE = 3
      ARM9_0: GEL Output: Module 4: UHPI               STATE = 3
      ARM9_0: GEL Output: Module 5: EMAC               STATE = 3
      ARM9_0: GEL Output: Module 6: DDR2 and SCR F3    STATE = 3
      ARM9_0: GEL Output: Module 7: MCASP0 + FIFO      STATE = 3
      ARM9_0: GEL Output: Module 8: SATA               STATE = 3
      ARM9_0: GEL Output: Module 9: VPIF               STATE = 3
      ARM9_0: GEL Output: Module 10: SPI 1              STATE = 3
      ARM9_0: GEL Output: Module 11: I2C 1              STATE = 3
      ARM9_0: GEL Output: Module 12: UART 1             STATE = 3
      ARM9_0: GEL Output: Module 13: UART 2             STATE = 3
      ARM9_0: GEL Output: Module 14: MCBSP0 + FIFO      STATE = 3
      ARM9_0: GEL Output: Module 15: MCBSP1 + FIFO      STATE = 3
      ARM9_0: GEL Output: Module 16: LCDC               STATE = 3
      ARM9_0: GEL Output: Module 17: eHRPWM (all)       STATE = 3
      ARM9_0: GEL Output: Module 18: MMC/SD 1           STATE = 3
      ARM9_0: GEL Output: Module 19: UPP                STATE = 3
      ARM9_0: GEL Output: Module 20: eCAP (all)         STATE = 3
      ARM9_0: GEL Output: Module 21: EDMA3 TC2          STATE = 3
      ARM9_0: GEL Output: Module 24: SCR-F0 Br-F0       STATE = 3
      ARM9_0: GEL Output: Module 25: SCR-F1 Br-F1       STATE = 3
      ARM9_0: GEL Output: Module 26: SCR-F2 Br-F2       STATE = 3
      ARM9_0: GEL Output: Module 27: SCR-F6 Br-F3       STATE = 3
      ARM9_0: GEL Output: Module 28: SCR-F7 Br-F4       STATE = 3
      ARM9_0: GEL Output: Module 29: SCR-F8 Br-F5       STATE = 3
      ARM9_0: GEL Output: Module 30: Br-F7 (DDR Contr)  STATE = 3
      ARM9_0: GEL Output: Module 31: L3 RAM, SCR-F4, Br-F6 STATE = 3

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • raneliya
      Posted by raneliya
      on May 29 2011 06:56 AM
      Genius5270 points

      Hi Daniel,

      In addition to the diagnostic information I gave before, When I compare the difference between the custom board to the EVM, I also see that the device ID in the board is:
      d800k006 - silicon revision 2.0 and in the EVM board: d800k004 - silicon revision 1.1 (difference in bootrom info category), there are also difference in device information category , maybe becuase the device id is different. There is no more difference in the other categories in the diagnostic information.
      As I undestand it is just the revision of the cpu - Meanwhile I have no idea why the custom board behaves different from the EVM.

      Regards,

      Ran

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • raneliya
      Posted by raneliya
      on Jun 03 2011 00:30 AM
      Verified Answer
      Verified by Daniel Allred
      Genius5270 points

      Hi,

       

      The issue was solved (after debug of UBL)  Any one interested can look at 

      http://e2e.ti.com/support/embedded/f/354/p/113807/405296.aspx#405296

       

      Ran

       

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • Daniel Allred
      Posted by Daniel Allred
      on Jun 03 2011 10:04 AM
      Genius15085 points

      Ran,

      Thanks for providing the update.  I think the lesson here is that the low-level boot loaders can be very much tied to the particulars of the board or platform, and therefore it is very likely that these will need to be customized for a custom platform.

      Regards, Daniel

      ----------------------------------------------------------------------------------------------------------
      Please click the
      Verify Answer button on this post if it answers your question.
      ----------------------------------------------------------------------------------------------------------

       

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    • jimmy zhang77361
      Posted by jimmy zhang77361
      on Apr 13 2012 03:14 AM
      Prodigy115 points

      Hi Ran:

      We also use AT45DB321D on our custom OMAP-L137 board. How did you add AT45DB321D support to spi-flash-writer? Can you share the modified spi-flash-writer code with us?

      You help is very appreciated!

       

      Jimmy

      Report Abuse
      • Reply
      You have posted to a forum that requires a moderator to approve posts before they are publicly available.
    12
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
    All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

    Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.