This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Here is the original message, which for some reason did not show up:
I am new to this forum. I need to get help with Serial Boot and Flash Loading Utility for OMAP-L138. I have rebuilt the code for my board, and it seems to communicate successfully, but when I try a command such as:
sfh_omap-L138 -p COM4 -flashType NAND -erase
to test erasing the flash, the communication works OK, but the target board does not erase the flash. There is no error message; the host thinks it was successful.
Any thoughts on how to debug this?
For that matter, did I even post this in the right place? If not, can someone tell me where I should have posted this question?
Thanks!
Mike