This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

when upp is working, you should not start EDMA, right?

ref this artical:

http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/114045.aspx

It said that upp will never emit "WAIT" signal in transfer.

so, if upp is working, we start a EDMA transfer,  the Upp transfer will be borken, right?

 

Is there an document talking about such conflicted peripherals?

  • The uPP peripheral has its own internal DMA that is separate from EDMA.  For this reason, using EDMA and uPP simultaneously should not be a problem.  TI has done testing to ensure that these activities do not interfere with each other.

     


    Please click the  Verify Answer  button on this post if it answers your question.

     

  • In reply to Joe Coombs:

    But on my board, I do observed that  EDMA affectting UPP.

    Maybe UPP peripheral 's speed is too high, FIFO is overflow.

  • In reply to twicave Feng:

    Are you operating the uPP peripheral at maximum speed (i.e. 75 MHz)?  If so, it is possible to encounter contention with other high-speed activity (such as EDMA transfers) on the internal system bus.  If possible, I recommend slowing the uPP clock speed to see if that alleviates the issue.

     


    Please click the  Verify Answer  button on this post if it answers your question.

     

  • In reply to Joe Coombs:

    Sorry for hijacking this post, but I am having this very same issue. UPP working as INPUT channel on an OMAP L138 (300MHz), UPP clock driven by the peripheral (FPGA) at 37.5MHz. As soon as I perform an EDMA3 transfer (from DDR into IRAM), UPP fails (i.e., I get an SIO_reclaim timeout error) even though the peripheral is still sending data.

    EDMA3 transfer routine is the edma3_poll_mode() from the examples. Tried edma3_int_mode() with the same results.

    Lowering the clock even more is not an option in this case.

    Ideas?

  • In reply to Carlos Vrancken:

    Perhaps try raising the UPP's priority in the MSTPRI registers.

    ---------------------------------------------------------------------------------------------------------
    http://processors.wiki.ti.com/index.php/User:BradGriffis
    --------------------------------------------------------------------------------------------------------- 

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.