Hi,
I operate the Spectrum Digital omap-l137 evaluation board with the DA830 audio daughterboard.
I hope my question is not off-topic here but I would not know where else to post my question.
The problem that I have is that the DA830 test code operates at a sampling frequency of 41700 Hz rather than 48 kHz. My intention is to modify the samplerate from 41700 to 48000 Hz but I do not know how to do this.
From the documentation of the ak4588 DAC used on the DA830 board (which is not a TI product, sorry) and the schematics of the DA830 board, I see that the MCLK is produced by the ak4588. The documentation says that MCLK is "512 x fs" and fs can be between 32 and 48 kHz if in single speed mode. Then, on the McAsp side I see that the LRCLK is produced by dividing the MCLK with a specific factor. And the LRCLK is fed back to the ak4588. Finally, for me, it seems that ak4588 has a sampling rate detection based on LRCLK which - again - controls the MCLK. This seems to be a control loop which is indeed undefined since the samplingrate was never specified anywhere.
Has anybody got any experience with this type of problem? Any idea what I need to do to change the samplingrate?
Thank you for any assistance,
best regards,
HT