Hi,
Referencing this post ( http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/95634.aspx#333192 ) can anyone confirm that Spi0 cannot be used on the L138 EVM because it shares lines with the ethernet PHY on the SOM?
Is this the case for all L138 SOM? Is there anyway around it?
I have a driver that works fine for Spi1, but change the base address to Spi0 and the clock and data appear highly mixed up. Have double checked pin and clock muxing, clock routing, for Spi0, etc
Thanks,
Matt