We want to send webcam input to touchscreen using gstreamer on OMAP-L138.

#gst-launch v4l2src always_copy=FALSE ! video/x-raw-yuv ! ffmpegcolorspace ! fbdevsink

outputs on stdout as:

Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock

----------------------------------------------------------------------

However, no input comes from the webcam.

Webcam is supported in UVC and a message appears as:
"usb 1-1: new full speed USB device using ohci and address 3
uvcvideo: Found UVC 1.00 device A4 tech USB2.0 Camera (0ac8:3420)"

when device plugged in.

- Do you have any suggestions about the problem?
- Does OMAP-L138 & Gstreamer compatibility cause this problem?
- Is it because of a package is missing?

Kind regards.