I use the OMAP-L138 to write/read DDR2, and I have problem.

1/  if I write some data to DDR2 and read from it right now when I have written, the first data which I read is wrong and the rest is OK, but if I write some data to DDR2 and has some time delay, then I read from it and I find that the all data I read is ok. I think is the problem concern with the time of convert between read and write, so I try to change the bit T_WTR in register SDTIMR1, but find that it no use, so I want to know is there some other bit in this register or other register can effect it?

I use the DDR2 is MT47H128M8CF-3, and the datawidth is 8, and I use 2 chip to compose a 16 bit datawidth referring to the page 129 in the datasheet of OMAP-L138, the clock rate is 150Mhz

The registers configuration is this

DDR->SDBCR = 0x00134632

                (DDR_DDR2EN --      1) 

                (DDR_DDREN --       1) 

                (DDR_SDRAMEN --     1)

                (DDR_NM --          1)     

                (DDR_CL --           3)      

                (DDR_IBANK --       3)   

                (DDR_PAGESIZE --   2);

               The other is 0

DDR->SDRCR =  0x00000492          

DDR->SDTIMR1 =   0x26922A09

(DDR_T_RFC --       19)              

                  (DDR_T_RP --        2) 

                  (DDR_T_RCD --       2)

                  (DDR_T_WR --        2) 

                  (DDR_T_RAS --       5)

                  (DDR_T_RC --        8)  

                  (DDR_T_RRD --       1) 

                  (DDR_T_WTR --       1);

DDR->SDTIMR2 =  0x3C14C722

(DDR_T_RASMAX --   7) 

                  (DDR_T_XP --         2)     

                  (DDR_T_XSNR --       20)   

                  (DDR_T_XSRD --       199)    

                  (DDR_T_RTP --         1)     

                  (DDR_T_CKE --         2);

2/  as I said above , I use 2 chip to compose a 16 bit datawidth referring to the page 129 in the datasheet of OMAP-L138 ,so is there anything(registers or bit in registers) I should notice particularly?

3/  there are some registers in DDR2 chip ,like < Standard Mode Register>< Extended Mode Register>, so should I configure these register in my program? Or I configure the 5 registers above and they can configure the Registers in DDR2chip automatically?

regards

xunliang