Hi,
I need to connect a FPGA to an OMAP L138. I can use the UPP port or the EMIFA. What are the advantages / inconvenient for each method ?
Thanks
Damien,
EMIFA interfaces with flash devices and SDRAM devices. In cases where FPGA interfaces with EMIFA, if you have other memory devices connected with peripheral, you could run into potential latency issues if you do not manage the memory access.
MityDSP is a device that connect an FPGA and a NAND flash to the EMIFA port. Here is a useful discussion on MityDSP that might interest you:
http://support.criticallink.com/redmine/boards/10/topics/562
You may also want to consider peripheral throughput and latencies before making your decision:
http://processors.wiki.ti.com/index.php/Device:OMAP-L138:Device_Evaluation#Peripheral_Throughput_and_Optimizations
Hope this helps.
Regards,
Rahul
---------------------------------------------------------------------------------Please click the Verify Answer button on this post if it answers your question.---------------------------------------------------------------------------------