Hi
We are devolping a product which has USB acting as slave.USB Slave connected to PC. Continuous Audio streaming happens from PC to USB Slave in full duplex mode(Upstream as well as downstream). As per OMAPl132 spec, the SoC supports the Isochronous transfer!!
My question whether the OMAPl132 has USB 2.0 Audio class driver support?
Kindly clarify me the above query
Regards
Vijayabharathi C
Hi, Anyone? I'd like to ask the same question.
Yan,
Its all about the class driver that you add to support USB Audio class. As long as its 2.0 and Isochronous transfers are supported, USB Audio Class should work, if the corresponding class driver exists in your code. Its supported in Linux. Assuming that you are using LInux.
-Renjith | www.pathpartnertech.com | Verify the answer if you think your query is resolved