Hello,
1). Does anybody know how to connect the data bus of an external ADC device to the UPP port if the data width is 12-bit? Should the 12-bit data bus connect to the 12 MSBs of UPP data or the 12 LSBs of the UPP data bus?
2). Can I connect the 12-bit ADC data to the UPP 12MSBs, i.e. D[15:4] if I set the UPP data interface to 16-bit interface (IWA=1), and the data width=12-bit (DPWA=4h)?
If the answer is YES, can I use the pin UPP_D[0] as an GPIO?
Thanks,
Wenbo