Hi,
I am trying to run an RTFS USB example on the Starter Kit OMAP-L137. The name of this project is : "RTFS_INSTALL_DIR/packages/ti/rtfs/example/usbhostmsc".
I plugged a USB memory stick into the USB1 (type A) port.
My USB stick is : PNY 1GB in FAT32 format.
All environment variables are OK.
The build is OK.
I modifyied the value of the #define "PSP_FILE_SYSTEM" at 1 in order to enable the Block Media driver to use RTFS.
But when I run, I have this message :
Initializing usb host stack
ohci_local0: OHCI version 1.0
ohci_local0: USB revision 1.0
ohci_local0: new device port=0 depth=0 speed=full
uhub0 Jungo Generic Root Hub, class 9/0, rev 0.11/af.00, addr 1
uhub0: 2 ports with 2 removable, self powered
musbhshc0: USB revision 2.0
musbhshc0: new device port=0 depth=0 speed=high
uhub1 Jungo Generic Root Hub, class 9/0, rev 0.20/af.00, addr 1
uhub1: 1 port with 1 removable, self powered
uhub0: new device port=1 depth=1 speed=full
ucompdev0 vendor 0x0930 USB Flash Memory, class 0/0, rev 2.00/1.00, addr 2
umass0 vendor 0x0930 USB Flash Memory, rev 2.00/1.00, addr 2
New disk attached as USB0
Assertion failed, (((pu && pu->plcwd))), file src/rtfscommon/source/rtkernfn.c, line 60
Someone can help me ? I am a begginer with USB...
Thank you.