Hi
Using VPIF, there is 3 types:
VPIF_IF_RAW_BAYER
VPIF_IF_BT1120
VPIF_IF_BT656
What's different about these?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Using VPIF, there is 3 types:
VPIF_IF_RAW_BAYER
VPIF_IF_BT1120
VPIF_IF_BT656
What's different about these?
Thanks.
Hi,
This is the interface type for vpif driver,
VPIF_IF_RAW_BAYER --> Indicates this interface/channel supports raw capture from sensor
VPIF_IF_BT1120 --> Indicates this interface/channel supports HD
VPIF_IF_BT656--> Indicates this interface/channel supports SD to be precise NTSC & PAL.
Thanks,
--Prabhakar Lad
Hi Prabhakar:
Thanks very much!
So If I want to support VideoStd_D1_PAL, I should select VPIF_IF_BT656?
Hi,
So If I want to support VideoStd_D1_PAL, I should select VPIF_IF_BT656? |
Yes you got it correct.
Thanks,
--Prabhakar Lad