I need to test whether the DDR2 is working on my custom board or not, by loading the gel files using ccs4. But i can't find a way to update the GEL files.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I need to test whether the DDR2 is working on my custom board or not, by loading the gel files using ccs4. But i can't find a way to update the GEL files.
Hi Taqi,
Thanks for your post.
Reusing/updating values in the Gel file would lead to read/write issues as the GEL file timings are specifically tuned for a particular memory chip and clock speed, instead, you can download the clocking spreadsheet from the below wiki and try calculating the values for the mDDR/DDR2 memory controller registers
http://processors.wiki.ti.com/index.php/Programming_mDDR/DDR2_EMIF_on_OMAP-L1x/C674x
The spreadsheet will automatically generate the values for the mDDR/DDR2 memory controller registers.
Thanks & regards,
Sivaraj K
Hi Sivaraj,
Thanks for your reply.
I have updated the GEL file using the Spreadsheet, but i am having few problems during debugging the GEL file. I have stated the problem in an other thread. can you please help me with that too ?
http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/335584.aspx