I am trying to Load GEL file on AM1808 processor using ccs4.
I have modified the PLL0 base address to 01C11000h to C1080000h, and also modified the DDR2 setting accordingly.
But when i start debug, the code stuck in an infinite loop.
/*Wait for the GOSTAT bit in PLLSTAT to clear to 0 (completion of phase alignment).*/
while(PLL0_PLLSTAT & 0x1==1) { }
and after a while the following output is shown in the console.
ARM9_0: Output: Memory Map Cleared.
ARM9_0: Output: ---------------------------------------------
ARM9_0: Output: Memory Map Setup Complete.
ARM9_0: Output: ---------------------------------------------
ARM9_0: Output: PSC Enable Complete.
ARM9_0: Output: ---------------------------------------------
ARM9_0: The GEL callback "OnTargetConnect()" is no longer running atomically
ARM9_0: Output: PLL0 init done for Core:300MHz, EMIFA:25MHz
ARM9_0: Output: mDDR initialization is in progress....
ARM9_0: Output: PLL1 init done for DDR:150MHz
ARM9_0: Output: Using mDDR settings
ARM9_0: Output: mDDR init for 150 MHz is done
ARM9_0: Output: ---------------------------------------------
ARM9_0: Output: DSP Wake Complete.
ARM9_0: Output: ---------------------------------------------
Is it a successful result or am i suppose to modify the gel file again ?