Hi
In dmai(DVSDK 4.03), after run:
/* Load the executable on the DSP */
status = PROC_load (processorId, dspExecutable, 0, NULL);
if (DSP_FAILED (status)) {
printf ("PROC_load () failed. Status = [0x%x]\n",
(Uint16)status) ;
retVal = -1;
goto DSPmsgqClose;
}
I got error, PROC_load return 0x8009! It means DSP_SDETACHED!
What's problem about this?
Does it need open DSP when system start?
Thanks very much!