Hi
I used omapl137evm spectrum digital.when i setup OMAPL137_dsp_1_00_00_11.exe, I see the following files :
C:\OMAPL137_dsp_1_00_00_11\REL_LSP_02_20_00_07\PSP_02_20_00_07\board_utilities\flash_writers\nand_writer
C:\OMAPL137_dsp_1_00_00_11\REL_LSP_02_20_00_07\PSP_02_20_00_07\board_utilities\flash_writers\spi_flash_writer
i want to write norflash on the da830 user interface board. i don't see any file for nor_writer.
can i download this file?
can i used OMAP-L137_FlashAndBootUtils_2_40 for norflash on the da830 user interface board?
in LSP_02.20_OMAP-L137_User_Guide.pdf i see "Flashing Boot Images to SPI Flash" and " Flashing Boot Images to NAND Flash". i don't see "Flashing Boot Images to NOR Flash". Please give me step by step instructions for "Flashing Boot Images to NOR Flash" and used norflash on the da830 user interface board ?
thank you