In previos work, CCS v3.3 was used but now I want to change CCS version v3.3 to v6.
in v3.3, if I click 'insert MEM' and type 'base' and 'len', I can add memory segment.
but in CCS v6, I can not add memory segment. It is 'add' button but there is no other menu.
OS : Win7 x64
CCS Version : 6
SYS/BIOS : 6_40_02_27
xdctools : 3_30_01_25_core
board : ZOOM OMAP-L138 EVM
how to add memory segment in ccs v6?