Dear e2e!
Is there anywhere a example of C/C++ program for external host processor, which loads TMS320C674x DSP via SPI.
Boot mode of TMS320C674x DSP is
SPI0/SPI1 Boot external host (Slave mode).
Yes, I have seen an algorithm of such program for external host in the SPRABB1C "Using the TMS320C6747/45/43 Bootloader".
But an example would be better....
Many thanks is advance!
Vitalii