Hi,
I read in the errata of the TMS320C6748 (sprz303h.pdf) that the McASP does not support inactive slots in combination with EDMA section 2.1.6). The errata makes me belief there is no workaround and it never works.
Is that true? Is it impossible to have two DSP's work together on a single I2S (TDM) bus?
I wanted to have one DSP do the left output and the other the right.
Are there plans to have this fixed?
Thanks in advance.
Kind regards,
Remco Poelstra