I use TMS320C6748 , fix-point fft how can to use?
I download fft.asm at address http://www.ti.com/lsds/ti/dsp/c6000_dsp/c674x/benchmarks.page#ffts ,but compiling result have a error:
'Building file: ../fft.asm'
'Invoking: C6000 Compiler'
"C:/ti/ccsv5/tools/compiler/c6000_7.4.4/bin/cl6x" -mv6740 --abi=coffabi -g --include_path="C:/ti/ccsv5/tools/compiler/c6000_7.4.4/include" --include_path="C:/ti/ccsv5/c6700/dsplib/Include" --include_path="/packages/ti/xdais" --include_path="/include" --define=c6748 --display_error_number --diag_warning=225 --diag_wrap=off --preproc_with_compile --preproc_dependency="fft.pp" "../fft.asm"
"../fft.asm", ERROR! at line 533: [E0802] Multi-cycle NOP instructions are illegal in the execute packet preceding an execute packet containing an SPKERNEL instruction.
SPKERNELR ;delay 0 cycles before reloading
1 Assembly Error, No Assembly Warnings
Errors in Source - Assembler Aborted
>> Compilation failure
gmake: *** [fft.obj] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****