I am using LCDK 6748 and a Leopard Imaging camera LI-CAM-OV5653-P33.
This camera has to use BT.1120 mode with operating clock at 74.25MHz.
I am using the " vpif lcd_loopback " which is in the C6748_StarterWare.
I think I need to change some parameters but I am not sure about which parameters I have to change.
I have changed:
Camera
#define CAPTURE_IMAGE_WIDTH (XXXX)
#define CAPTURE_IMAGE_HEIGHT (XXXX)
I have put the camera pixels resolutions.
Also, I have changed in the VPIFCaptureModeConfig(), with the struct vbufParam of the BT.1120 mode.
I do not know where I have to change the clock frecuency and if I need to change more parameters.
After doing this, the led screen is green but the screen is still blank.
Can you help me?
Thank you.
Kind Regards .