Hello All,
I am facing issue while executing the ARM binary code from External memory (SRAM interface over EMIFB bus) using Code Composer Studio.
The HW Environment is OMAP L137 based customized HW & SRAM is interfaced to EMIFB bus using FPGA.
Below are the steps followed:
1) In order execute the ARM code from SRAM, I have modified the DSP GEL file and configured the required interfaces.
2) Connected to DSP Core so that GEL file gets executed.
3) Generated ARM binary file where all code segments are moved to SRAM locations. Connected and loaded the binary onto ARM core.
4) Upon loading the binary, the ARM core entering into “Running” state instead of halting
at main( ). When I press the “pause” button, the control is halting at invalid location.
Can you please help me in resolving this issue.
Thanks & Regards
Srinivas