Hi ,
I'm developing on OMAP-L137 EVM.
The ADC/DAC is controlled by AIC3106.
When I set register 93 (refer to below image), I could volume up/down the sound of Line Out.
But when I set register 93, the ADC/DAC will halt. After finish resetting AIC3106, ADC/DAC could keep running....
In the above way, I have to halt my program and wait for AIC3106 reset.
Is there other way to dynamically volume up/down (Don't halt program )?