Hi,
In a recent project we replaced the obsolete SD card with a new one and now the SD card can be accessed only in debug mode.
I want to write the specifications of the SD cards briefly as a class under "functioning" and "non-functioning" ones
Functioning SD Card spec:
Controller : SMI Controller
Flash IC : Samsung SLC_NAND Flash IC
Non-functioning SD Card spec :
Controller : ITE Controller
Flash IC : Toshiba SLC_NAND Flash IC
Any feedback about such an issue is appreciated.