Hi,
I´m new to programming DSPs and learning with the OMAPL138 LCDK.
Is there an example about an EDMA usage for the CCS6 with the newest TI-RTOS.
I just found older versions for EDMA examples. Thanks for your replies.
Yours sincerly
Christoph
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I´m new to programming DSPs and learning with the OMAPL138 LCDK.
Is there an example about an EDMA usage for the CCS6 with the newest TI-RTOS.
I just found older versions for EDMA examples. Thanks for your replies.
Yours sincerly
Christoph
Hi Christoph,
Please refer to the following TI E2E post.
http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/p/362531/1273971.aspx#1273971
http://software-dl.ti.com/dsps/dsps_public_sw/sdo_tii/psp/edma3_lld/index.html
Hi,
Thanks for your post.
I don't think, there are examples for EDMA usage with the newest TI-RTOS & CCSv6 and again, there are no examples available for OMAPL138 boards with latest TI-RTOS, but available examples can be ported to other boards and devices. Please check the TI-RTOS porting guide as below:
http://processors.wiki.ti.com/index.php/TI-RTOS_Porting_Guide
If you plan to use TI-RTOS within Code Composer Studio v6.0 or higher, is it recommended that you
use the CCS App Center to install TI-RTOS. Please download the latest version of TI-RTOS as below:
http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/mcusdk/index.html
http://processors.wiki.ti.com/index.php/TI-RTOS#Examples
Kindly check the release notes as below:
Thanks & regards,
Sivaraj K
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
-------------------------------------------------------------------------------------------------------
Hi Christoph,
there are examples for EDMA3 LLD driver for SYS/BIOS 6. I am not sure about the latest versions.
But I recently installed these versions:
BIOS 6.37.01.24
EDMA3 LLD 2.11.09.08
SysLink 2.21.02.10
Regards,
Jiri
Hi Jiri,
thank you for your reply. I found the example in the edma folder, but I can´t watch the source files. I installed the 7.2.3 compiler in the meantime. When i want to open the files
Error retrieving content description for resource 'edma_drv_bios6_omapl138-st-sample/dma_chain_test.c'.
occurs, and i can´t watch the files. What do I do wrong?
Regards,
Christoph
Christoph,
after the installation you should get the directory like this:
...
├── examples
│ ├── CSL2_DAT_DEMO
│ │ ├── demo
│ │ │ └── evmDA830
│ │ ├── docs
│ │ │ ├── CSL_DAT_Adapter.ppt
│ │ │ └── readme.txt
│ │ └── src
│ │ ├── bios6_adapter
│ │ ├── csl2_legacy_include
│ │ └── dat_edma3LLD
│ └── edma3_driver
...
│ ├── evmOMAPL138
│ │ ├── makefile
│ │ ├── rtsc_config
│ │ └── sample_app
│ ├── evmOMAPL138_ARM
│ │ ├── makefile
│ │ ├── rtsc_config
│ │ └── sample_app
...
│ └── src
│ ...
│ ├── dma_chain_test.c
│ ...
│ ├── main.c
│ ├── qdma_link_test.c
│ ├── qdma_test.c
│ └── sample.h
├── makerules
│ ├── build_config.mk
│ ├── common.mk
│ ├── docs
│ │ └── makerules_spec.pdf
│ ├── env.mk
│ ├── platform.mk
│ ├── rules_64p.mk
│ ├── rules_64t.mk
│ ├── rules_66.mk
│ ├── rules_674.mk
│ ├── rules_arm9.mk
│ ├── rules_CS_a8.mk
│ ├── rules_m3.mk
│ └── rules_TI_a8.mk
...
I highlighted the files the most relevant to the building example
Have you got the same structure?
Jiri