OMAP L138, I want to open a read file using
fp = fopen(InputData.txt,"r"); // read mode
but it didn't seem to work! How should i create/read/write file in AMR memory?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
OMAP L138, I want to open a read file using
fp = fopen(InputData.txt,"r"); // read mode
but it didn't seem to work! How should i create/read/write file in AMR memory?
Hi David,
I don't know what is AMR memory,
I think you meant ARM memory right ?
What are you trying to do ?
Is that ARM app or DSP app ?
Are you working with Linux sw or something else like bare-metal code (starterware) ?
If it is linux, you would get lot of examples in internet for that (file manipulation).
Also we have "nand writer" CCS project that has file manipulation support such as fread, fopen, fclose etc.,
// Setup pointer in RAM aisPtr = (Uint8 *) UTIL_allocMem(aisAllocSize); // Clear memory for (i=0; i<aisAllocSize; i++) aisPtr[i]=0xFF; // Go to start of file fseek(fPtr,0,SEEK_SET); // Read file data if (aisFileSize != fread(aisPtr, 1, aisFileSize, fPtr)) { DEBUG_printString("\tWARNING: File Size mismatch.\r\n"); } // Close file fclose (fPtr);