Hi,
m unable to load cmemk.ko module into the kernel, I get following when i try to run video_copy example.
./loadmodules.sh
cmemk: disagrees about version of symbol struct_module
dsplinkk: no version for "struct_module" found: kernel tainted.
insmod: error inserting 'cmemk.ko': -1 Invalid module format
DSPLINK Module (1.61.03) created on Date: Apr 16 2009 Time: 18:37:45
root@10.110.6.102:/opt/codec_engine/video_copy# ./app.out
App-> Application started.
CMEM Error: init: Failed to open /dev/cmem: 'No such file or directory'
@0x000d77d9:[T:0x4001df50] OM - Memory_init> ERROR: Failed to initialize CMEM
@0x000d9d66:[T:0x40969490] OP - Processor_create_d> Loading and starting DSP server 'video_copy.x674' FAILED, status=[0x80008008] (look for error code 'DSP_EBASE + 0x8' in dsp
@0x000d9eb5:[T:0x40969490] OP - Processor_delete_d> Closing remote transport FAILED, status=0x80008002.
@0x000d9f8a:[T:0x40969490] OP - Processor_delete_d> Stopping DSP FAILED, status=0x80008002
@0x000da04d:[T:0x40969490] OP - Processor_delete_d> Closing pool FAILED, status=0x80008000
@0x000da0e1:[T:0x40969490] OP - Processor_delete_d> Detaching from DSP FAILED, status=0x80008000
@0x000da167:[T:0x40969490] OP - Processor_delete_d> Destroying DSP FAILED, status=0x80008000
@0x000da251:[T:0x4001df50] CE - rserverOpen: can't start 'video_copy.x674'; Processor_create failed
CEapp-> ERROR: can't open engine video_copy
App-> Application FAILED.
any suggestion will be appreciated
With best regards,
Ravi