Hi;
My application needs real time image processing for optical sorting on dsp kit without intermediate PC.
the multicore c6678 have no camera interfaces so,
is OMAP L138 LCDK board and processor are capable for my application to process 30 fps D1 resolution color images?
As following link ,
http://www.ti.com/lit/ml/sprt634/sprt634.pdf
is it the VGA port can used as input from camera ?
what about the Leopard Imaging camera sensor input (32- pin ZIP connector)
is it line camera sensor or some interface for external camera?
if TI has such a DSP development board, which having on board camera and video output. if so ,please suggest.
Thanks,