I am using a ZOOM OMAP-L138 EVM development Kit with the OMAPL138B processor chip.
I am trying to get the ndk_evmOMAPL138_arm9_helloWorld Example program working but am encountering the following error:
This project was created using a version of XDCtools that is not currently installed: 3.20.3.63. Please install the XDCtools of this version, or migrate the project to one of the supported versions.
When I try to install XDCtools Version 3.20.3.63 I get this:
Is there either a way to update the project to use Version 3.30.3.47 of the XDCtools or to fix the install problem with version 3.20.3.63.