Hello,
We are planning to use the OMAP-L138 capability to interface with a SATA device.
So I have couple of questions regarding this:
1) What is the minimum hardware needed to have the OMAP boot and communicate with the SATA device? Please advise if the below components are sufficient:
a) necessary circuitry to drive the signals on necessary device pins (reset, NMI, JTAG pins, EMU0, EMU1, RTCK, PLL pins, RTC pins, DEEPSLEEP, Boot Mode Selection, SATA pins, VCCs and GND).
b) crystal oscillators connected to :24MhZ (OSCIn: L19, OSCOUT: K19) and 32.768 Khz (RTC_XI:J19, RTC_XO:H19)
c) Booting device: Can we use raw NAND? If so, Can you please send me the instructions to create a booting image in the RAW NAND?
2) We are planning to use the OMAP-L138 DSP+ARM9™Development Kit as a starting point. In which case can you please send us an example project that have the necessary functions to communicate with a SSD device (to do erase/program/read functions) .
Thanks,
Ayman