Please clarify the size of the CS0 to CS5 and DDR2 on the OMAPL138-EP memory map.
From the OMAPL138-EP datasheet, the EMIFA chip select 2 to 5 have 32K size. Is that 32KB? Can you confirm that. Chip select 3 is for NAND boot. Does this mean, NAND flash cannot be larger than 32KB?
I want to use the following
4Gbit NAND flash on CS3 for OMAP boot.
ASRAM interface on CS2. What is the size of this and max address I can use?
DDR2. What is the max size for this? The memory map indicates 512M.