Hello.
In case OmapL138, It is difficult to find infomation regarding the speed of Shared-memory(128KB internal, Memory map: 0x8000 0000 ~ 0x8001 0000).
which is faster Shared-Memory(128KB Internal) or DDR(External 150MHz)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello.
In case OmapL138, It is difficult to find infomation regarding the speed of Shared-memory(128KB internal, Memory map: 0x8000 0000 ~ 0x8001 0000).
which is faster Shared-Memory(128KB Internal) or DDR(External 150MHz)?
Hi Hyun-geun,
All of the on-chip memory including the shared RAM should be able to be accessed faster than external memory i.e DDR.
Please refer below mentioned post, this will give you more clear idea,
e2e.ti.com/.../976044