Hi,
I am trying to build an example of IPC (Notify (ARM)) with Logic evaluation board (OMAP 138 Soc) through SYS-BIOS v6.
Once I build the project in CCS V6 I start getting these errors.
Description Resource Path Location Type
#10010 errors encountered during linking; "Notify_ARM.out" not built Notify_ARM C/C++ Problem
<a href="file:/c:/ti/ccsv6/tools/compiler/dmed/HTML/10234.html">#10234-D</a> unresolved symbols remain Notify_ARM C/C++ Problem
Undefined reference to 'ti_sdo_ipc_gates_GateMPSupportNull_query__E' in file C:\Users\ITE6320\IPC_omap_SysBios_workspace_v6_1\Notify_ARM\Debug\configPkg\package\cfg\notify_arm_pe9.oe9 .xdchelp /Notify_ARM C/C++ Problem
Undefined reference to 'ti_sdo_ipc_gates_GatePeterson_query__E' in file C:\Users\ITE6320\IPC_omap_SysBios_workspace_v6_1\Notify_ARM\Debug\configPkg\package\cfg\notify_arm_pe9.oe9 .xdchelp /Notify_ARM C/C++ Problem
Undefined reference to 'ti_sdo_ipc_heaps_HeapMemMP_isBlocking__E' in file C:\Users\ITE6320\IPC_omap_SysBios_workspace_v6_1\Notify_ARM\Debug\configPkg\package\cfg\notify_arm_pe9.oe9 .xdchelp /Notify_ARM C/C++ Problem
I click on one of the error and I receive a quick fix pop up window saying
try adding the following line to the configuration file "notify_arm.cfg" in project notiy_arm
var ti_sdo_ipc_gates_GateMPSupportNull = xdc.useModule('ti.sdo.ipc.gates.GateMPSupportNull');
but no solution even with adding these files to the cfg file.
here are the version I am using to build the example
XDC 3.31.0.24
SYS BIOS 641.4.54
IPC 1.25.3.15
I tried many versions combination but I had similar errors.
please advise
Thanks for the support