BOARD : OMAP-L138
TOOL : CCS v3.3
pspdrivers_01_30_00_06
dspbios : 5.33.06
I want to use GPIO bank interrupt.
this is bank8 pin8 interrupt init function.
and this is bank interrupt block.
I connect function generator(1Hz square signal) to GPIO8_8 pin. and compile -> program -> run....
program doesn't go to "IO_Bank8_isr"..
give me some advice.