1 Can I only modify the linux kernal source code about this ? If it was,where could I change?
2 I have a project about UBL which I can open in CCS3.3. Can I compile it in CCS3.3 and then load it into nandflash ?
3 I try to compile the project about UBL in CCS3.3. It is sucessful,but it can not run well after I load it. The cld screen is blank and the console can not reciece any output. How can I debug this progect?