Hi,
I have a custom designed board that has 128Mbyte DDR2( Micron MT47H64M16HR-3T ). I want to use 256Mbyte DDR2 (Micron MT47H128M16RT-25E).
After assemly process, i prepared a u-boot code (but this is same with 128Mbyte vesion) and generated an bin file using AISgen D800K008 for boot from UART.
But it doesn't work. Is there any example and document to increase DDR2 capacity?
Do i need to change u-boot for Uart boot mode?
In my design i connect DDR_A[13] and do i need to change Pinmux for this pin?
My new valuef for DDR2 register as follow:
Clock : 300 Mhz
DRPYC1R : 0x00000044
SDCR : 0x00134632
SDTIMR1 : 0x3A523209
SDTIMR2: 0x7C1EC722
SDRCR : 0x00000492