Hi i used below hardware : 1. omapl137evm ( rev g ) i used below software : 1. dsplink-1_61_03-prebuilt 2. bios_setuplinux_5_33_05 3. ti_cgt_c6000_6.1.9_setup_linux_x86 4. xdctools_setuplinux_3_10_05_61 5. pspdrivers_01_30_00_05 6. OMAPL137_arm_setuplinux_1_00_00_11 7.kernel 2.6.18 ////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// i want used MSGQ and NOTIFY for transfer message and CHNL for transfer data between arm and dsp in omapl137evm with dsplink. ////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// i used this code for armside. ////////////////////////////////////////////////////////////////////////////////////////////////////////////////// // INCLUDES ///////////////////////////////////////////////////////////////////////////////////////////////////////////////// #include <dsplink.h> #include <proc.h> #include <chnl.h> #include <msgq.h> #include <pool.h> #include <SDSP.h> #include <system_os.h> #include <stdio.h> #include <stdio.h> #include <unistd.h> #include <sys/types.h> #include <sys/stat.h> #include <fcntl.h> #include <linux/delay.h> #include <asm/segment.h> #include <string.h> #include <stdlib.h> #include <dirent.h> #include <assert.h> #include <sys/mman.h> #include <notify.h> #include <signal.h> #define DDRVNAME "dsp" #define IC_NAME(drvName) drvName #define OC_NAME(drvName) drvName #define IC IC_NAME(DDRVNAME) #define OC OC_NAME(DDRVNAME) ////////////////////////////////////////////////////////////////////////////////////////////////////////////////// // FOR POOLING ///////////////////////////////////////////////////////////////////////////////////////////////////////////////// #define NUM_ARGS 2 #define ARG_SIZE 256 #define SAMPLE_POOL_ID 0 #define NUMMSGPOOLS 4 #define NUMMSGINPOOL0 2 #define NUMMSGINPOOL1 2 #define NUMMSGINPOOL2 1 #define NUMMSGINPOOL3 4 #define APP_BUFFER_SIZE DSPLINK_ALIGN (sizeof (ControlMsg), DSPLINK_BUF_ALIGN) ////////////////////////////////////////////////////////////////// #define DATA_LEN 256 #define DATA_LEN_Byte (DATA_LEN*4) STATIC Uint32 SCALE_BufferSizeOut = DSPLINK_ALIGN (DATA_LEN_Byte,DSPLINK_BUF_ALIGN); STATIC Uint32 SCALE_BufferSizeIn = DSPLINK_ALIGN (DATA_LEN_Byte,DSPLINK_BUF_ALIGN); STATIC Char8 * SCALE_BuffersIn [1] ; STATIC Char8 * SCALE_BuffersOut[1] ; STATIC ChannelIOInfo SCALE_IOReqIn,SCALE_IOReqOut; #define CHNL_ID_OUTPUT 0 #define CHNL_ID_INPUT 1 ////////////////////////////////////////////////////////////////// static char notify_status = 0; static char ReceiveFlag = 0; static char mode = 0; typedef struct ControlMsg { MSGQ_MsgHeader header; Uint16 command; Char8 arg1[ARG_SIZE]; } ControlMsg; ControlMsg *msg; DSP_STATUS status = DSP_SOK; Uint8 processorId = 0; Uint16 msgId = 0; char EndFlag1 = 0; char EndFlag2 = 0; Char8 arg1[ARG_SIZE]; Char8 printmessage[ARG_SIZE]; void sendControlMsg(Uint16 cmd,Char8 *arg1); void signalHandler(int sig); #define USERINPUTMAXNUMCHARS 70 #define DELIMITERS " " #if defined ZCPY_LINK #define SAMPLEMQT_CTRLMSG_SIZE ZCPYMQT_CTRLMSG_SIZE STATIC ZCPYMQT_Attrs mqtAttrs; #endif STATIC Uint32 SampleBufSizes[NUMMSGPOOLS] = { APP_BUFFER_SIZE, SAMPLEMQT_CTRLMSG_SIZE, DSPLINK_ALIGN (sizeof(MSGQ_AsyncLocateMsg),DSPLINK_BUF_ALIGN), DSPLINK_ALIGN (DATA_LEN_Byte,DSPLINK_BUF_ALIGN) }; STATIC Uint32 SampleNumBuffers[NUMMSGPOOLS] = { NUMMSGINPOOL0, NUMMSGINPOOL1, NUMMSGINPOOL2, NUMMSGINPOOL3 }; #if defined ZCPY_LINK STATIC SMAPOOL_Attrs SamplePoolAttrs = { NUMMSGPOOLS, SampleBufSizes, SampleNumBuffers, FALSE }; #endif ///////////////////////////////////////////////////////////////////////////////////////////////////////////////// // Message Naming ///////////////////////////////////////////////////////////////////////////////////////////////////////////////// STATIC Char8 SampleGppMsgqName[DSP_MAX_STRLEN] = "GPPMSGQ1"; STATIC Char8 SampleDspMsgqName[DSP_MAX_STRLEN] = "DSPMSGQ"; STATIC MSGQ_Queue SampleGppMsgq = (Uint32) MSGQ_INVALIDMSGQ; STATIC MSGQ_Queue SampleDspMsgq = (Uint32) MSGQ_INVALIDMSGQ; Char8 dspMsgqName[DSP_MAX_STRLEN]; ///////////////////////////////////////////////////////////////////////////////////////////////////////////////// // FOR LOADING ///////////////////////////////////////////////////////////////////////////////////////////////////////////////// extern LINKCFG_Object LINKCFG_config; STATIC NORMAL_API Void MP_LIST_Notify (IN Uint32 eventNo, IN OPT Pvoid arg, IN OPT Pvoid info) ; /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// // INITIALIZATION /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// NORMAL_API DSP_STATUS DSP_Create(IN Char8* dspExecutable, IN Char8* strNumIterations, IN Uint8 processorId) { Uint32 numArgs = NUM_ARGS; MSGQ_LocateAttrs syncLocateAttrs; Char8* args[NUM_ARGS]; ChannelAttrs chnlAttrInput ; ChannelAttrs chnlAttrOutput ; SYSTEM_0Print("Entered DSP_Create ()\n"); ////////////////////////////// //PROC_attach ////////////////////////////// status = PROC_setup(NULL); if (DSP_SUCCEEDED(status)) { status = PROC_attach(processorId, NULL); if (DSP_FAILED(status)) { SYSTEM_1Print("PROC_attach () failed. Status = [0x%x]\n", status); } } ////////////////////////////// //POOL_open ////////////////////////////// if (DSP_SUCCEEDED(status)) { status = POOL_open(POOL_makePoolId(processorId, SAMPLE_POOL_ID), &SamplePoolAttrs); if (DSP_FAILED(status)) { SYSTEM_1Print("POOL_open () failed. Status = [0x%x]\n", status); } } else { SYSTEM_1Print("PROC_setup () failed. Status = [0x%x]\n", status); } ////////////////////////////// //MSGQ_open ////////////////////////////// if (DSP_SUCCEEDED(status)) { status = MSGQ_open(SampleGppMsgqName, &SampleGppMsgq, NULL); if (DSP_FAILED(status)) { SYSTEM_1Print("MSGQ_open () failed. Status = [0x%x]\n", status); } } ////////////////////////////// //MSGQ_setErrorHandler ////////////////////////////// if (DSP_SUCCEEDED(status)) { status = MSGQ_setErrorHandler(SampleGppMsgq, POOL_makePoolId(processorId, SAMPLE_POOL_ID)); if (DSP_FAILED(status)) { SYSTEM_1Print("MSGQ_setErrorHandler () failed. Status = [0x%x]\n", status); } } ////////////////////////////// //Set the notifier ////////////////////////////// if (DSP_SUCCEEDED(status)) { status = NOTIFY_register (processorId, 0, 5, (FnNotifyCbck) MP_LIST_Notify, 0) ; if (DSP_FAILED (status)) { SYSTEM_1Print ("NOTIFY_register() failed. Status = [0x%x]\n", status) ; } } ////////////////////////////// //PROC_load ////////////////////////////// if (DSP_SUCCEEDED(status)) { args [0] = strNumIterations; { status = PROC_load(processorId, dspExecutable, numArgs, args); } if (DSP_FAILED(status)) { SYSTEM_1Print("PROC_load () failed. Status = [0x%x]\n", status); } } ////////////////////////////// //Create a channel to DSP ////////////////////////////// if (DSP_SUCCEEDED (status)) { chnlAttrOutput.mode = ChannelMode_Output ; chnlAttrOutput.endianism = Endianism_Default ; chnlAttrOutput.size = ChannelDataSize_32bits ; status = CHNL_create (processorId, CHNL_ID_OUTPUT, &chnlAttrOutput); if (DSP_FAILED (status)) { SYSTEM_1Print("CHNL_create (CHNL_ID_OUTPUT) failed. Status = [0x%x]\n", status) ; } else { SYSTEM_0Print("CHNL_create (CHNL_ID_OUTPUT) success.\n") ; } } ////////////////////////////// //Create a channel from DSP ////////////////////////////// if (DSP_SUCCEEDED (status)) { chnlAttrInput.mode = ChannelMode_Input ; chnlAttrInput.endianism = Endianism_Default ; chnlAttrInput.size = ChannelDataSize_32bits ; status = CHNL_create (processorId, CHNL_ID_INPUT, &chnlAttrInput) ; if (DSP_FAILED (status)) { SYSTEM_1Print("CHNL_create () failed. Status = [0x%x]\n", status) ; } else { SYSTEM_0Print("CHNL_create (CHNL_ID_INPUT) success.\n") ; } } /////////////////////////////////////////////////// //Allocate buffer(s) for data transfer to DSP. /////////////////////////////////////////////////// if (DSP_SUCCEEDED (status)) { status = CHNL_allocateBuffer ( processorId, CHNL_ID_OUTPUT, SCALE_BuffersOut, //Pointer to receive array of allocated buffers SCALE_BufferSizeOut , //Size of each buffer 1) ; //Number of buffers to allocate if (DSP_FAILED (status)) { SYSTEM_1Print("CHNL_allocateBuffer (1) failed. Status = [0x%x]\n",status); } else { SYSTEM_0Print("CHNL_allocateBuffer (1) success.\n"); } } if (DSP_SUCCEEDED (status)) { status = CHNL_allocateBuffer ( processorId, CHNL_ID_INPUT, SCALE_BuffersIn, //Pointer to receive array of allocated buffers SCALE_BufferSizeIn , //Size of each buffer 1) ; //Number of buffers to allocate if (DSP_FAILED (status)) { SYSTEM_1Print("CHNL_allocateBuffer (2) failed. Status = [0x%x]\n",status); } else { SYSTEM_0Print("CHNL_allocateBuffer (2) success.\n"); } } ////////////////////////////// //PROC_start ////////////////////////////// if (DSP_SUCCEEDED(status)) { status = PROC_start(processorId); if (DSP_FAILED(status)) { SYSTEM_1Print("PROC_start () failed. Status = [0x%x]\n", status); } else { SYSTEM_0Print("PROC_start () success.\n"); } } ////////////////////////////// //MSGQ_transportOpen ////////////////////////////// if (DSP_SUCCEEDED(status)) { mqtAttrs.poolId = POOL_makePoolId(processorId, SAMPLE_POOL_ID); status = MSGQ_transportOpen(processorId, &mqtAttrs); if (DSP_FAILED(status)) { SYSTEM_1Print("MSGQ_transportOpen () failed. Status = [0x%x]\n", status); } else { SYSTEM_0Print("MSGQ_transportOpen () success.\n"); } } ////////////////////////////// //MSGQ_locate ////////////////////////////// if (DSP_SUCCEEDED(status)) { syncLocateAttrs.timeout = WAIT_FOREVER; status = DSP_ENOTFOUND; SYSTEM_2Sprint(dspMsgqName, "%s%d", (Uint32) SampleDspMsgqName, processorId); while ((status == DSP_ENOTFOUND) || (status == DSP_ENOTREADY)) { status = MSGQ_locate(dspMsgqName, &SampleDspMsgq, &syncLocateAttrs); if ((status == DSP_ENOTFOUND) || (status == DSP_ENOTREADY)) { SYSTEM_0Print("DSP_ENOTFOUND || DSP_ENOTREADY.\n"); SYSTEM_Sleep(100000); } else if (DSP_FAILED(status)) { SYSTEM_1Print("MSGQ_locate () failed. Status = [0x%x]\n", status); } } } SYSTEM_0Print("Finish DSP_Create ()\n"); return status; } /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// // EXECUTION /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// NORMAL_API DSP_STATUS DSP_Execute(IN Uint32 numIterations, Uint8 processorId) { char *ptr; char inbuf[USERINPUTMAXNUMCHARS]; int i; Uint32 AudioPtrSize; Int32 *AudioPtrBuff; SYSTEM_0Print("Entered DSP_Execute ()\n"); sprintf(printmessage,"ARM :Wake UP\n"); SYSTEM_0Print(printmessage); (void) signal(SIGINT, signalHandler); SYSTEM_0Print("Entered DSP_SUCCEEDED ()\n") ; if (DSP_SUCCEEDED (status)) { SCALE_IOReqIn.buffer = SCALE_BuffersIn [0] ; SCALE_IOReqIn.size = SCALE_BufferSizeIn; SCALE_IOReqOut.buffer= SCALE_BuffersOut [0] ; SCALE_IOReqOut.size = SCALE_BufferSizeOut; } ////////////////////////////// //Receive Message ////////////////////////////// status = MSGQ_get(SampleGppMsgq,WAIT_FOREVER, (MsgqMsg *) &msg); if (DSP_FAILED(status)) { SYSTEM_1Print("MSGQ_get () failed. Status = [0x%x]\n", status); } if (msg->command == 0x01) { SYSTEM_1Print("DSP :%s\n", (Uint32) msg->arg1); sprintf(arg1,"Blink"); sprintf(printmessage,"ARM :BLINK_GPIO012\n"); SYSTEM_0Print(printmessage); sendControlMsg(0x0a,arg1); } notify_status = 0; ReceiveFlag = 1; while ( EndFlag1 == 0 ) { while ( EndFlag2 == 0 ) { SYSTEM_0Print("ARM :Enter_Command = "); fgets( inbuf, USERINPUTMAXNUMCHARS, stdin ); ptr = strtok( inbuf, DELIMITERS ); usleep(1000); if ( EndFlag2 == 0 ) { switch ( *ptr ) { case 'a': { ///////////////////////////////////////////// // Send Message ///////////////////////////////////////////// sprintf(arg1,"GPIO_0_12"); sprintf(printmessage,"ARM :BLINK_GPIO012\n"); SYSTEM_0Print(printmessage); sendControlMsg(0x0a,arg1); *ptr = 0; break; } case 'b': { ///////////////////////////////////////////// // Send Message ///////////////////////////////////////////// sprintf(arg1,"GPIO_0_13"); sprintf(printmessage,"ARM :BLINK_GPIO013\n"); SYSTEM_0Print(printmessage); sendControlMsg(0x0b,arg1); *ptr = 0; break; } case 'c': { ///////////////////////////////////////////// // Send Message ///////////////////////////////////////////// sprintf(arg1,"GPIO_0_14"); sprintf(printmessage,"ARM :BLINK_GPIO014\n"); SYSTEM_0Print(printmessage); sendControlMsg(0x0c,arg1); *ptr = 0; break; } case 'd': { ///////////////////////////////////////////// // Send Message ///////////////////////////////////////////// sprintf(arg1,"Data_transfer"); sprintf(printmessage,"ARM :Data_transfer\n"); SYSTEM_0Print(printmessage); sendControlMsg(0x0d,arg1); ///////////////////////////////////////////// // Build Data ///////////////////////////////////////////// AudioPtrBuff = (Int32 *) (SCALE_IOReqIn.buffer); for ( i=0 ; i<DATA_LEN ; i++ ) { *AudioPtrBuff = 5; AudioPtrBuff++; } AudioPtrSize = (SCALE_IOReqIn.size); ///////////////////////////////////////////// // Issue 'filled' buffer to the channel. ///////////////////////////////////////////// status = CHNL_issue (processorId,CHNL_ID_OUTPUT,&SCALE_IOReqIn); if (DSP_FAILED (status)) { SYSTEM_1Print ("CHNL_issue (CHNL_ID_OUTPUT) failed. Status = [0x%x]\n",status) ; } ////////////////////////////////////////////// // Reclaim 'empty' buffer from the channel ////////////////////////////////////////////// status = CHNL_reclaim (processorId,CHNL_ID_OUTPUT,2000,&SCALE_IOReqIn); if (DSP_FAILED (status)) { SYSTEM_1Print ("CHNL_reclaim (CHNL_ID_OUTPUT) failed. Status = [0x%x]\n",status) ; } /////////////////////////////////////////////// // Issue 'empty' buffer to the channel. /////////////////////////////////////////////// status = CHNL_issue (processorId,CHNL_ID_INPUT,&SCALE_IOReqOut); if (DSP_FAILED (status)) { SYSTEM_1Print ("CHNL_issue (CHNL_ID_INPUT) failed. Status = [0x%x]\n",status) ; } ///////////////////////////////////////////////// // Reclaim 'filled' buffer from the channel ///////////////////////////////////////////////// status = CHNL_reclaim (processorId,CHNL_ID_INPUT,2000,&SCALE_IOReqOut) ; if (DSP_FAILED (status)) { SYSTEM_1Print ("CHNL_reclaim (CHNL_ID_INPUT) failed. Status = [0x%x]\n",status) ; } ///////////////////////////////////////////// // Print 20 Receive Data ///////////////////////////////////////////// AudioPtrBuff=(Int32 *)SCALE_IOReqOut.buffer; AudioPtrSize=(SCALE_IOReqOut.size); for ( i=0 ; i<20 ; i++ ) { SYSTEM_1Print("%d,\n", (Uint32)(*AudioPtrBuff)); AudioPtrBuff++; } //////////////////////////////////////////////////////// status = DSP_SOK; *ptr = 0; break; } case 'e': { notify_status = 0; sprintf(arg1,"EXIT"); sprintf(printmessage,"ARM :TURN OFF\n"); SYSTEM_0Print(printmessage); sendControlMsg(0x0e,arg1); *ptr = 0; EndFlag2 = 1; break; } } } } if ( notify_status == 1 ) { notify_status = 0; ReceiveFlag = 0; EndFlag1 = 1; if (mode == 0x02) { SYSTEM_1Print("DSP :%s\n", (Uint32) msg->arg1); } } } usleep(1000); SYSTEM_0Print("Finish DSP_Create ()\n"); return status; } /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// // FINALIZATION /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// NORMAL_API Void DSP_Delete(Uint8 processorId) { DSP_STATUS tmpStatus = DSP_SOK; SYSTEM_0Print("Entered DSP_Delete ()\n"); ////////////////////////////// //MSGQ_release ////////////////////////////// status = MSGQ_release(SampleDspMsgq); if (DSP_FAILED(status)) { SYSTEM_1Print("MSGQ_release () failed. Status = [0x%x]\n", status); } ////////////////////////////// //MSGQ_transportClose ////////////////////////////// tmpStatus = MSGQ_transportClose(processorId); if (DSP_SUCCEEDED(status) && DSP_FAILED(tmpStatus)) { status = tmpStatus; SYSTEM_1Print("MSGQ_transportClose () failed. Status = [0x%x]\n", status); } ////////////////////////////// //PROC_stop ////////////////////////////// tmpStatus = PROC_stop(processorId); if (DSP_SUCCEEDED(status) && DSP_FAILED(tmpStatus)) { status = tmpStatus; SYSTEM_1Print("PROC_stop () failed. Status = [0x%x]\n", status); } ////////////////////////////// //Unregister notification ////////////////////////////// tmpStatus = NOTIFY_unregister (processorId, 0, 5, (FnNotifyCbck) MP_LIST_Notify, 0) ; if (DSP_SUCCEEDED (status) && DSP_FAILED (tmpStatus)) { status = tmpStatus ; SYSTEM_1Print ("NOTIFY_unregister () failed. Status = [0x%x]\n", status) ; } ////////////////////////////// //MSGQ_setErrorHandler ////////////////////////////// tmpStatus = MSGQ_setErrorHandler(MSGQ_INVALIDMSGQ, MSGQ_INVALIDMSGQ); if (DSP_SUCCEEDED(status) && DSP_FAILED(tmpStatus)) { status = tmpStatus; SYSTEM_1Print("MSGQ_setErrorHandler () failed. Status = [0x%x]\n", status); } ////////////////////////////// //MSGQ_close ////////////////////////////// tmpStatus = MSGQ_close(SampleGppMsgq); if (DSP_SUCCEEDED(status) && DSP_FAILED(tmpStatus)) { status = tmpStatus; SYSTEM_1Print("MSGQ_close () failed. Status = [0x%x]\n", status); } ////////////////////////////// //POOL_close ////////////////////////////// tmpStatus = POOL_close(POOL_makePoolId(processorId, SAMPLE_POOL_ID)); if (DSP_SUCCEEDED(status) && DSP_FAILED(tmpStatus)) { status = tmpStatus; SYSTEM_1Print("POOL_close () failed. Status = [0x%x]\n", status); } ////////////////////////////// //PROC_detach ////////////////////////////// tmpStatus = PROC_detach(processorId); if (DSP_SUCCEEDED(status) && DSP_FAILED(tmpStatus)) { status = tmpStatus; SYSTEM_1Print("PROC_detach () failed. Status = [0x%x]\n", status); } ////////////////////////////// //PROC_destroy ////////////////////////////// tmpStatus = PROC_destroy(); if (DSP_SUCCEEDED(status) && DSP_FAILED(tmpStatus)) { status = tmpStatus; SYSTEM_1Print("PROC_destroy () failed. Status = [0x%x]\n", status); } SYSTEM_0Print("Finish DSP_Delete ()\n"); } /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// // MAIN /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// NORMAL_API Void DSP_Main(IN Char8* dspExecutable, IN Char8* strNumIterations, IN Char8* strProcessorId) { Uint32 numIterations = 0; Uint8 processorId = 0; if (LINKCFG_config.dspConfigs[processorId]->dspObject->doDspCtrl == DSP_BootMode_Boot_Pwr) { SYSTEM_0Print("DSP_BootMode_Boot_Pwr\n"); } else if ( LINKCFG_config.dspConfigs[processorId]->dspObject->doDspCtrl == DSP_BootMode_NoBoot) { SYSTEM_0Print("DSP_BootMode_NoBoot\n"); } if ((dspExecutable != NULL) && (strNumIterations != NULL)) { numIterations = SYSTEM_Atoi(strNumIterations); if (numIterations > 0xFFFF) { status = DSP_EINVALIDARG; SYSTEM_1Print("ERROR! Invalid arguments specified.\n Max iterations = %d\n", 0xFFFF); } else { processorId = SYSTEM_Atoi(strProcessorId); if (processorId >= MAX_DSPS) { SYSTEM_1Print("== Error: Invalid processor id %d specified ==\n", processorId); status = DSP_EFAIL; } if (DSP_SUCCEEDED(status)) { status = DSP_Create(dspExecutable, strNumIterations, processorId); if (DSP_SUCCEEDED(status)) { status = DSP_Execute(numIterations, processorId); } DSP_Delete(processorId); } } } else { status = DSP_EINVALIDARG; SYSTEM_0Print("ERROR! Invalid arguments specified for DSP application\n"); } } //////////////////////////////////////////////////////////////////////////////////////////////// STATIC NORMAL_API Void MP_LIST_Notify (IN Uint32 eventNo,IN OPT Pvoid arg,IN OPT Pvoid info) { notify_status = 1; if ( ReceiveFlag == 1 ) { ////////////////////////////// //Receive Message ////////////////////////////// status = MSGQ_get(SampleGppMsgq,WAIT_FOREVER,(MsgqMsg *)&msg); if (DSP_FAILED(status)) { SYSTEM_1Print("MSGQ_get () failed. Status = [0x%x]\n",status); } else { mode = msg->command; } } return; } void sendControlMsg( unsigned short int cmd,Char8 *arg1) { ////////////////////////////// //send message ////////////////////////////// if (DSP_SUCCEEDED(status)) { msgId = MSGQ_getMsgId(msg); MSGQ_setMsgId(msg, msgId); msg->command = cmd; sprintf(msg->arg1,arg1); status = MSGQ_put(SampleDspMsgq,(MsgqMsg) msg); if (DSP_FAILED(status)) { MSGQ_free((MsgqMsg) msg); SYSTEM_1Print("MSGQ_put () failed. Status = [0x%x]\n", status); } } if (DSP_SUCCEEDED (status)) { status = NOTIFY_notify (processorId,0,5,(Uint32) 0); if (DSP_FAILED (status)) { SYSTEM_1Print ("NOTIFY_notify () failed."" Status = [0x%x]\n",status) ; } } return; } void signalHandler(int sig) { sprintf(arg1,"EXIT"); sprintf(printmessage,"ARM :TURN OFF\n"); SYSTEM_0Print(printmessage); sendControlMsg(0x0e,arg1); EndFlag2 = 1; usleep(1000); } ////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// i used below code for dspside : /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// // INCLUDES /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// #include "SDSPcfg.h" #include <gbl.h> #include <sys.h> #include <sem.h> #include <msgq.h> #include <pool.h> #include <notify.h> #include <dsplink.h> #include <platform.h> #include <failure.h> #include "SDSP_config.h" #include "tskMessage.h" #include <stdio.h> #include <string.h> #include <std.h> #include <sio.h> #include <gio.h> #include <iom.h> #include <sys.h> #include <tsk.h> #include <idl.h> #include <ecm.h> #include <mem.h> #include <log.h> #include <c64.h> #include <c6x.h> #include <ti/pspiom/cslr/cslr_gpio.h> #include <ti/pspiom/cslr/soc_OMAPL137.h> #include <ti/pspiom/gpio/Gpio.h> #include <dio.h> #include <iom.h> extern TSKMESSAGE_TransferInfo* info; ControlMsg* msg; Char arg1[ARG_SIZE]; Int sendControlMsg( Uint16 cmd,Char *arg1,TSKMESSAGE_TransferInfo* info); /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// // DSPLINK PARAMETERS /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// volatile char notify_flag = 0; volatile char mode = 0; #define FILEID FID_APP_C Uint8 dspMsgQName[DSP_MAX_STRLEN]; extern Uint16 numTransfers; static Void TSKMPLIST_notify (Uint32 eventNo, Ptr arg, Ptr notifyinfo) ; ///////////////////// GPIO CONFIGURATION ////////////////////////////// #define LOW 0x0 #define HIGH 0x1 #define GPIO_BANK_1 0x00 #define GPIO0_12_PIN 13 #define GPIO0_13_PIN 14 #define GPIO0_14_PIN 15 #define GPIO0_15_PIN 16 extern Gpio_Handle gpio; //////////////////////////////////////////////////////////////////////////////////////////////////////////////////// #define DSPLINK_DRVNAME "/dio_dsplink" #define INPUT_CHNL_NAME(drvName) drvName ## "0" #define OUTPUT_CHNL_NAME(drvName) drvName ## "1" #define INPUT_CHANNEL INPUT_CHNL_NAME(DSPLINK_DRVNAME) #define OUTPUT_CHANNEL OUTPUT_CHNL_NAME(DSPLINK_DRVNAME) SIO_Handle inputStream,outputStream ; #define DATA_LEN 256 #define DATA_LEN_Byte (DATA_LEN*4) Uint32 bufferSize = DATA_LEN_Byte; Uint32 numBuffers = 1; Char * buffer1 ; Char * buffer2 ; ////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// // GPIO CONFIGURATION FUNCTION ////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// Int GpioConfiguration(Void) { Int status = SYS_OK; Gpio_PinCmdArg UserPinCmdArg; UserPinCmdArg.pin = GPIO0_12_PIN; UserPinCmdArg.value = Gpio_Direction_Output; Gpio_setPinDir(gpio,&UserPinCmdArg); UserPinCmdArg.pin = GPIO0_12_PIN; UserPinCmdArg.value = HIGH; Gpio_setPinVal(gpio,&UserPinCmdArg); UserPinCmdArg.pin = GPIO0_13_PIN; UserPinCmdArg.value = Gpio_Direction_Output; Gpio_setPinDir(gpio,&UserPinCmdArg); UserPinCmdArg.pin = GPIO0_13_PIN; UserPinCmdArg.value = HIGH; Gpio_setPinVal(gpio,&UserPinCmdArg); UserPinCmdArg.pin = GPIO0_14_PIN; UserPinCmdArg.value = Gpio_Direction_Output; Gpio_setPinDir(gpio,&UserPinCmdArg); UserPinCmdArg.pin = GPIO0_14_PIN; UserPinCmdArg.value = HIGH; Gpio_setPinVal(gpio,&UserPinCmdArg); UserPinCmdArg.pin = GPIO0_15_PIN; UserPinCmdArg.value = Gpio_Direction_Output; Gpio_setPinDir(gpio,&UserPinCmdArg); UserPinCmdArg.pin = GPIO0_15_PIN; UserPinCmdArg.value = HIGH; Gpio_setPinVal(gpio,&UserPinCmdArg); return status; } /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// // INITIALIZATION /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// Int TSKMESSAGE_create(Void) { Int status = SYS_OK; SIO_Attrs attrs = SIO_ATTRS; MSGQ_Attrs msgqAttrs = MSGQ_ATTRS; MSGQ_LocateAttrs syncLocateAttrs; ////////////////////////////// //message allocating ////////////////////////////// info = MEM_calloc(DSPLINK_SEGID, sizeof(TSKMESSAGE_TransferInfo), DSPLINK_BUF_ALIGN); if (info == NULL) { status = SYS_EALLOC; SET_FAILURE_REASON(status); } else { info->numTransfers = numTransfers; info->localMsgq = MSGQ_INVALIDMSGQ; info->locatedMsgq = MSGQ_INVALIDMSGQ; } ////////////////////////////////////////////////// //Register notification for the event callback ///////////////////////////////////////////////// if (status == SYS_OK) { status = NOTIFY_register (ID_GPP, 0, 5, (FnNotifyCbck) TSKMPLIST_notify, info) ; if (status != SYS_OK) { SET_FAILURE_REASON (status) ; } } //////////////////////////////////////// //Create Input and Output Streams /////////////////////////////////////// if (status == SYS_OK) { attrs.nbufs = numBuffers; attrs.segid = DSPLINK_SEGID; attrs.align = DSPLINK_BUF_ALIGN; attrs.flush = TRUE ; attrs.model = SIO_ISSUERECLAIM; attrs.timeout = 2000; inputStream = SIO_create (INPUT_CHANNEL,SIO_INPUT,bufferSize,&attrs); outputStream = SIO_create (OUTPUT_CHANNEL,SIO_OUTPUT,bufferSize,&attrs); if ((inputStream == NULL) || (outputStream == NULL)) { status = SYS_EALLOC ; SET_FAILURE_REASON (status) ; } } //////////////////////////////////////// //Allocating Buffers /////////////////////////////////////// if (status == SYS_OK) { status = POOL_alloc (SAMPLE_POOL_ID,(Ptr *) &buffer1,bufferSize) ; if (status != SYS_OK) { SET_FAILURE_REASON (status) ; } } if (status == SYS_OK) { status = POOL_alloc (SAMPLE_POOL_ID,(Ptr *) &buffer2,bufferSize) ; if (status != SYS_OK) { SET_FAILURE_REASON (status) ; } } if (status == SYS_OK) { SEM_new(&(info->notifySemObj), 0); msgqAttrs.notifyHandle = &(info->notifySemObj); msgqAttrs.pend = (MSGQ_Pend) SEM_pendBinary; msgqAttrs.post = (MSGQ_Post) SEM_postBinary; SYS_sprintf((Char *)dspMsgQName, "%s%d", DSP_MSGQNAME, GBL_getProcId()); ////////////////////////////// //message open ////////////////////////////// status = MSGQ_open((String)dspMsgQName, &info->localMsgq, &msgqAttrs); if (status != SYS_OK) { SET_FAILURE_REASON(status); } else { ////////////////////////////// //MSGQ_setErrorHandler ////////////////////////////// MSGQ_setErrorHandler(info->localMsgq, SAMPLE_POOL_ID); status = SYS_ENOTFOUND; while ((status == SYS_ENOTFOUND) || (status == SYS_ENODEV)) { syncLocateAttrs.timeout = SYS_FOREVER; ////////////////////////////// //MSGQ_locate ////////////////////////////// status = MSGQ_locate(GPP_MSGQNAME, &info->locatedMsgq, &syncLocateAttrs); if ((status == SYS_ENOTFOUND) || (status == SYS_ENODEV)) { TSK_sleep(1000); } } } info->sequenceNumber = 0; } return status; } /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// // EXECUTION /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// Int TSKMESSAGE_execute(Void) { Int status = SYS_OK; Char * Audio_In = (Char *) buffer1; Char * Audio_Out = (Char *) buffer2; Arg arg = 0; Int nmadus; Int receivedSize; int i; Gpio_PinCmdArg UserPinCmdArg; char EndFlag1 = 0; char EndFlag2 = 0; char EndFlag3 = 0; char EndFlag4 = 0; char EndFlag5 = 0; ///////////////////////////// //allocating message //////////////////////////// status = MSGQ_alloc(SAMPLE_POOL_ID, (MSGQ_Msg*) &msg, APP_BUFFER_SIZE); ////////////////////////////// //send message ////////////////////////////// if (status == SYS_OK) { SYS_sprintf(arg1,"Wake UP"); sendControlMsg(0x01,arg1,info); } ////////////////////////////// //GPIO CONFIGURATION ////////////////////////////// GpioConfiguration(); if (status == SYS_OK) { while ( EndFlag1 == 0 ) { switch (mode) { case 0x0a: { while ( EndFlag2 == 0 ) { UserPinCmdArg.pin = GPIO0_12_PIN; UserPinCmdArg.value = LOW; Gpio_setPinVal(gpio,&UserPinCmdArg); TSK_sleep(1000); UserPinCmdArg.pin = GPIO0_12_PIN; UserPinCmdArg.value = HIGH; Gpio_setPinVal(gpio,&UserPinCmdArg); TSK_sleep(1000); if ( notify_flag == 1 ) { if (status == SYS_OK) { switch (mode) { case 0x0b: { EndFlag2 = 1; break; } case 0x0c: { EndFlag2 = 1; break; } case 0x0d: { EndFlag2 = 1; break; } case 0x0e: { EndFlag1 = 1; EndFlag2 = 1; SYS_sprintf(arg1,"TURN OFF"); sendControlMsg(0x02,arg1,info); break; } } } else { SET_FAILURE_REASON (status); } notify_flag = 0; } } EndFlag2 = 0; break; } case 0x0b: { while ( EndFlag3 == 0 ) { UserPinCmdArg.pin = GPIO0_13_PIN; UserPinCmdArg.value = LOW; Gpio_setPinVal(gpio,&UserPinCmdArg); TSK_sleep(1000); UserPinCmdArg.pin = GPIO0_13_PIN; UserPinCmdArg.value = HIGH; Gpio_setPinVal(gpio,&UserPinCmdArg); TSK_sleep(1000); if ( notify_flag == 1 ) { if (status == SYS_OK) { switch (mode) { case 0x0a: { EndFlag3 = 1; break; } case 0x0c: { EndFlag3 = 1; break; } case 0x0d: { EndFlag3 = 1; break; } case 0x0e: { EndFlag1 = 1; EndFlag3 = 1; SYS_sprintf(arg1,"TURN OFF"); sendControlMsg(0x02,arg1,info); break; } } } else { SET_FAILURE_REASON (status); } notify_flag = 0; } } EndFlag3 = 0; break; } case 0x0c: { while ( EndFlag4 == 0 ) { UserPinCmdArg.pin = GPIO0_14_PIN; UserPinCmdArg.value = LOW; Gpio_setPinVal(gpio,&UserPinCmdArg); TSK_sleep(1000); UserPinCmdArg.pin = GPIO0_14_PIN; UserPinCmdArg.value = HIGH; Gpio_setPinVal(gpio,&UserPinCmdArg); TSK_sleep(1000); if ( notify_flag == 1 ) { if (status == SYS_OK) { switch (mode) { case 0x0a: { EndFlag4 = 1; break; } case 0x0b: { EndFlag4 = 1; break; } case 0x0d: { EndFlag4 = 1; break; } case 0x0e: { EndFlag1 = 1; EndFlag4 = 1; SYS_sprintf(arg1,"TURN OFF"); sendControlMsg(0x02,arg1,info); break; } } } else { SET_FAILURE_REASON (status); } notify_flag = 0; } } EndFlag4 = 0; break; } case 0x0d: { while ( EndFlag5 == 0 ) { /////////////////////////////////////////////// // Issue 'empty' buffer to the channel. /////////////////////////////////////////////// status = SIO_issue (inputStream,Audio_In,bufferSize,arg); if (status == SYS_OK) { ///////////////////////////////////////////////// // Reclaim 'filled' buffer from the channel ///////////////////////////////////////////////// nmadus = SIO_reclaim (inputStream,(Ptr *) &Audio_In,&arg); receivedSize = nmadus; } ///////////////////////////////////////////// // Processing Data ///////////////////////////////////////////// for ( i=0 ;i<DATA_LEN ; i++ ) { Audio_Out[i] = 2 * Audio_In[i]; } /////////////////////////////////////////////// // Issue 'filled' buffer to the channel. /////////////////////////////////////////////// status = SIO_issue (outputStream,Audio_Out,receivedSize,arg); if (status == SYS_OK) { ///////////////////////////////////////////////// // Reclaim 'empty' buffer from the channel ///////////////////////////////////////////////// SIO_reclaim (outputStream,(Ptr *)&(Audio_Out),&arg); } status = SYS_OK; if ( notify_flag == 1 ) { if (status == SYS_OK) { switch (mode) { case 0x0a: { EndFlag5 = 1; break; } case 0x0b: { EndFlag5 = 1; break; } case 0x0c: { EndFlag5 = 1; break; } case 0x0e: { EndFlag1 = 1; EndFlag5 = 1; SYS_sprintf(arg1,"TURN OFF"); sendControlMsg(0x02,arg1,info); break; } } } else { SET_FAILURE_REASON (status); } notify_flag = 0; } } EndFlag5 = 0; break; } } } UserPinCmdArg.pin = GPIO0_12_PIN; UserPinCmdArg.value = HIGH; Gpio_setPinVal(gpio,&UserPinCmdArg); UserPinCmdArg.pin = GPIO0_13_PIN; UserPinCmdArg.value = HIGH; Gpio_setPinVal(gpio,&UserPinCmdArg); UserPinCmdArg.pin = GPIO0_14_PIN; UserPinCmdArg.value = HIGH; Gpio_setPinVal(gpio,&UserPinCmdArg); UserPinCmdArg.pin = GPIO0_15_PIN; UserPinCmdArg.value = HIGH; Gpio_setPinVal(gpio,&UserPinCmdArg); TSK_sleep(100); } else { SET_FAILURE_REASON (status); } return status; } /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// // FINALIZATION /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// Int TSKMESSAGE_delete(Void) { Int status = SYS_OK; Int tmpStatus = SYS_OK; Bool freeStatus = FALSE; ////////////////////////////// //MSGQ_release ////////////////////////////// if (info->locatedMsgq != MSGQ_INVALIDMSGQ) { status = MSGQ_release(info->locatedMsgq); if (status != SYS_OK) { SET_FAILURE_REASON(status); } } ////////////////////////////// //MSGQ_setErrorHandler ////////////////////////////// MSGQ_setErrorHandler(MSGQ_INVALIDMSGQ, POOL_INVALIDID); ////////////////////////////// //MSGQ_close ////////////////////////////// if (info->localMsgq != MSGQ_INVALIDMSGQ) { tmpStatus = MSGQ_close(info->localMsgq); if ((status == SYS_OK) && (tmpStatus != SYS_OK)) { status = tmpStatus; SET_FAILURE_REASON(status); } } ////////////////////////////// //Unregister notification ////////////////////////////// status = NOTIFY_unregister (ID_GPP,0,5,(FnNotifyCbck) TSKMPLIST_notify,info) ; if (status != SYS_OK) { SET_FAILURE_REASON (status) ; } ////////////////////////////// //MEM_free ////////////////////////////// freeStatus = MEM_free(DSPLINK_SEGID, info, sizeof(TSKMESSAGE_TransferInfo)); if ((status == SYS_OK) && (freeStatus != TRUE)) { status = SYS_EFREE; SET_FAILURE_REASON(status); } return status; } /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// // NOTIFICATION /////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// static Void TSKMPLIST_notify (Uint32 eventNo, Ptr arg, Ptr notifyinfo) { (Void) eventNo ; (Void) notifyinfo ; (Void) arg ; notify_flag = 1; MSGQ_get(info->localMsgq,(MSGQ_Msg*) &msg,SYS_FOREVER); mode = msg->command; TSK_sleep(10); return; } Int sendControlMsg( Uint16 cmd,Char *arg1,TSKMESSAGE_TransferInfo* info) { Int status = SYS_OK; ////////////////////////////// //send message ////////////////////////////// msg->command = cmd; SYS_sprintf(msg->arg1,arg1); info->sequenceNumber++; if (info->sequenceNumber == MSGQ_INTERNALIDSSTART) { info->sequenceNumber = 0; } MSGQ_setMsgId((MSGQ_Msg) msg, info->sequenceNumber); MSGQ_setSrcQueue((MSGQ_Msg) msg, info->localMsgq); status = MSGQ_put(info->locatedMsgq,(MSGQ_Msg) msg); if (status != SYS_OK) { SET_FAILURE_REASON(status); } else { NOTIFY_notify (ID_GPP,0,5,(Uint32) 0); } return status; } ////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// when we run the code, we can see below message : "ARM :Enter_Command = " ////////////////////////////////////////////////////////////////////////////////////////////////////////// if i put "a" => dsp do blinking gpio_0_12 i can see the user led 1 on the omapl137 evm start blinking and every thing is ok. if i put "b" => dsp do blinking gpio_0_13 i can see the user led 2 on the omapl137 evm start blinking and every thing is ok. if i put "c" => dsp do blinking gpio_0_14 i can see the user led 3 on the omapl137 evm start blinking and every thing is ok. if i put "d" => arm transfer 256 word to dsp with CHNL function, then dsp do process data and transfer 256 word to arm with SIO function, i see below errors : "CHNL_reclaim (CHNL_ID_OUTPUT) failed." "CHNL_reclaim(CHNL_ID_INPUT) failed." then arm print receive data that is wrong!!!!! /////////////////////////////////////////////////////////////////////////////////////////////////////// in my code MSGQ and NOTIFY is ok but i cant transfer data with CHNL. i don't know which is wrong in my code. please help to fix this problem. Thank you Regards, Mahdi