Hi
I used omapl137evm from spectrum digital.
i used below example from ti :
C:\Program Files\Texas Instruments\pspdrivers_01_30_00_05\packages\ti\pspiom\examples\evmOMAPL137\uart\interrupt\build\uartSample.pjt
this example run on my board very good.
in this example when data transmit with uart, program wait in below line until receive 1000 byte :
status = GIO_submit(hUart_OUT,IOM_WRITE, buf, &len, NULL);
i will not wait in line. i want do my work but when data is send for me i get it.
can i do this work with interrupt function?
can i used this line in interrupt function?
Regards,
Mahdi