At this point I don't think I have a problem with the HW but a configuration mistake on my side. I'm trying to debug in another thread why I can't boot from UART2 on an omap-l137 and after reading a few other threads its seems that it is a good idea to run the Gel Debug script. I'm running in CCS6 but I'm not able to get what I'm expecting.
This is what I do:
1-)create a dummy project to the ARM or the DSP, the basic main template. That allows me to open a debug session. =
2-) once in the debug session I load the new Gel file and the go to the scripts->run all and I get the following output
ARM9_0: GEL Output:
---------------------------------------------
ARM9_0: GEL Output: | Device Information |
ARM9_0: GEL Output: ---------------------------------------------
ARM9_0: GEL Output: DEV_INFO_00 = 0x9B7DF02F
ARM9_0: GEL Output: DEV_INFO_01 = 0x00000000
ARM9_0: GEL Output: DEV_INFO_02 = 0x0000F3F2
ARM9_0: GEL Output: DEV_INFO_03 = 0x00000022
ARM9_0: GEL Output: DEV_INFO_04 = 0x00000000
ARM9_0: GEL Output: DEV_INFO_05 = 0x000003E0
ARM9_0: GEL Output: DEV_INFO_06 = 0x00000080
ARM9_0: GEL Output: DEV_INFO_07-DEV_INFO_08-DEV_INFO_09-DEV_INFO_10-DEV_INFO_11-DEV_INFO_12 = 8-0-153998-25-20-35
ARM9_0: GEL Output: DEV_INFO_13,DEV_INFO_14,DEV_INFO_15,DEV_INFO_16 = 0,0,0,5726
ARM9_0: GEL Output: -----
ARM9_0: GEL Output: DEV_INFO_17 = 0x00030003
ARM9_0: GEL Output: DEV_INFO_18 = 0x00000000
ARM9_0: GEL Output: DEV_INFO_19 =ARM9_0: GEL Output: 0ARM9_0: GEL Output: 0ARM9_0: GEL Output: 0ARM9_0: GEL Output: 0ARM9_0: GEL Output: 0ARM9_0: GEL Output:
ARM9_0: GEL Output: -----
ARM9_0: GEL Output: DEV_INFO_20 = 0x30303864
ARM9_0: GEL Output: DEV_INFO_21 = 0x3330306B
ARM9_0: GEL Output: DEV_INFO_22 = 0x30303864
ARM9_0: GEL Output: DEV_INFO_23 = 0x3330306B
ARM9_0: GEL Output: -----
ARM9_0: GEL Output: DEV_INFO_24 = 0x19023014
ARM9_0: GEL Output: DEV_INFO_25 = 0x0802598E
ARM9_0: GEL Output: DEV_INFO_06 = 0x00000080
ARM9_0: GEL Output: DEV_INFO_26 = 0x2CBC0000
ARM9_0: GEL Output:
ARM9_0: GEL Output: ---------------------------------------------
ARM9_0: GEL Output: | BOOTROM Info |
ARM9_0: GEL Output: ---------------------------------------------
Run_All() cannot be evaluated.
condition does not evaluate to a value
at rom_id=(arm_dsp ? *((unsigned int *) 0xFFFD000c) : *((unsigned int *) 0x1170000c)) [OMAPL1x_debug.gel:88]
at Print_ROM_Info() [OMAPL1x_debug.gel:65]
at Run_All()
I think what I'm doing wrong is how I'm connecting to the target. The wiki instructs to:
processors.wiki.ti.com/.../OMAP-L1x_Debug_Gel_Files
- Connect to the processor, can be ARM or DSP of any OMAP-L1x, AM1x, or TMS320C674x device.
- Tools -> Gel Files
- Right-click on the window and select "Load Gel"
- Go to Scripts -> Diagnostics -> Run All
how do I connect to the processor? any suggestions?