root@tl:/sys/devices/platform/leds-gpio.1/leds/user_led1# ls
brightness device max_brightness power subsystem trigger uevent
root@tl:/sys/devices/platform/leds-gpio.1/leds/user_led1# cat brightness
255
In the LED driver, the content in file "brightness" indicates the LED is light or not.
if the LED flicker quickly for a long time, will it reduce the FLASH life?
Or the file "brightness" is just exist in RAM?