This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Thanks for your post.
Please download quickStart_OMAPL1x_rCSL_2.0 from the below download wiki which describes the available examples for both the OMAPL137 and OMAPL138 EVMs and there is an example synopsis which provides an overview of each available example.
http://processors.wiki.ti.com/index.php/QuickStartOMAPL1x_rCSL#rCSL_Examples
I think, you will find the gpio_multi_led_interrupt, TIMER_led_blink_frequency, McASPEcho and other sample examples but McASPEcho example would be available only for OMAPL138 EVM and not OMAPL137, so, you would require porting efforts to change the example from L138 to L137 through which you could walkthrough the code for ADC initialization.
Thanks & regards,
Sivaraj K
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
--------------------------------------------------------------------------------------------------------