I am excited to start implementing a project that involves using the OMAP L138 LCDK, but I need guidance about how to begin interfacing with the LCDK. I have been reading the wikis (MCDSK User Guide and L138 LCDK), but I have not yet succsefully compiled and ran code.
- Do I need a hardware Emulator to accomplish this task?
- Will any of the suggested Emulators (XDS100, XDS200, XDS510, XDS560) suffice for this task?
- Which interfaces on the LCDK can be used to send I2C and SPI?
- Where can I found a pinout for the Expansion socket on the LCDK?
- If an Emulator is not required, how do I transfer, and execute CCS code on the LCDK?
- How can I load one of the sample DSP applications to the LCDK? The MCSDK OMAPL138 tutorial instructs to: << Create new Target "mcsdk.ccxml" with "Spectrum Digital XDS510USB Emulator" as Connection and "LCSDKOMAPL138" as Board or Device. >> within CCS.
- Where can I find the Reference Manual for writing code for the OMAP L138 LCDK?
Thank you in advance for any guidance you can provide!