I am trying to cross compile Linux kernel for OMAP L138 as per the document provided by SDK for OMAP L138. My host PC is 64bit Ubuntu 12
I am facing problem fixdep: error fstat'ing depfile: scripts/basic/.fixdep.d: Invalid argument. I have attached the output when I am trying to make defconfig
[linux-devkit]:/home/jagadish/arm-linux-3.1.10/linux-3.1.10> ARCH=arm CROSS_COMPILE=arm-arago-linux-gnueabi- make omapl138_lcdk_defconfig
HOSTCC scripts/basic/fixdep
In file included from /opt/ti-sdk-omapl138-lcdk-01.00.00/linux-devkit/arm-arago-linux-gnueabi/usr/include/stdlib.h:955:0,
from scripts/basic/fixdep.c:112:
/opt/ti-sdk-omapl138-lcdk-01.00.00/linux-devkit/arm-arago-linux-gnueabi/usr/include/bits/stdlib.h:65:1: warning: no previous prototype for ‘ptsname_r’ [-Wmissing-prototypes]
In file included from /opt/ti-sdk-omapl138-lcdk-01.00.00/linux-devkit/arm-arago-linux-gnueabi/usr/include/netinet/in.h:24:0,
from /opt/ti-sdk-omapl138-lcdk-01.00.00/linux-devkit/arm-arago-linux-gnueabi/usr/include/arpa/inet.h:23,
from scripts/basic/fixdep.c:116:
/opt/ti-sdk-omapl138-lcdk-01.00.00/linux-devkit/arm-arago-linux-gnueabi/usr/include/stdint.h:153:0: warning: "__INT64_C" redefined [enabled by default]
<built-in>:0:0: note: this is the location of the previous definition
/opt/ti-sdk-omapl138-lcdk-01.00.00/linux-devkit/arm-arago-linux-gnueabi/usr/include/stdint.h:154:0: warning: "__UINT64_C" redefined [enabled by default]
<built-in>:0:0: note: this is the location of the previous definition
In file included from /opt/ti-sdk-omapl138-lcdk-01.00.00/linux-devkit/arm-arago-linux-gnueabi/usr/include/sys/socket.h:40:0,
from /opt/ti-sdk-omapl138-lcdk-01.00.00/linux-devkit/arm-arago-linux-gnueabi/usr/include/netinet/in.h:25,
from /opt/ti-sdk-omapl138-lcdk-01.00.00/linux-devkit/arm-arago-linux-gnueabi/usr/include/arpa/inet.h:23,
from scripts/basic/fixdep.c:116:
/opt/ti-sdk-omapl138-lcdk-01.00.00/linux-devkit/arm-arago-linux-gnueabi/usr/include/bits/socket.h:427:23: warning: ‘struct mmsghdr’ declared inside parameter list [enabled by default]
/opt/ti-sdk-omapl138-lcdk-01.00.00/linux-devkit/arm-arago-linux-gnueabi/usr/include/bits/socket.h:427:23: warning: its scope is only this definition or declaration, which is probably not what you want [enabled by default]
fixdep: error fstat'ing depfile: scripts/basic/.fixdep.d: Invalid argument
make[1]: *** [scripts/basic/fixdep] Error 2
make: *** [scripts_basic] Error 2
Kindly help me.
Thanks & regards,
Jagadish Haldar