Sorry if this is the wrong forum, but it appears as if the OMAP forums are read only.
While trying to setup a PWM output, I find the term "SYSCLKOUT" through-out the eHRPWM section of the datasheet. However, the term is not found anywhere else in the datasheet. The description for SYSCLKOUT is the system clock. This is somewhat ambiguous, but one could possibly extrapolate the meaning as being the ARM core clock which means the clock source for the eHRPWM section is PLL0_SYSCLK2 or PLL1_SYSCLK2 (depending on other settings).
Is this the actual source of the clock for the eHRPWM module ?
It looks like this entire section of the datasheet was lifted out of a TMS320 document and dropped in the OMAP document.
Thanks---