Dear Friends,
I'm using the MCBSP_MasterExampleProject example available at:
C:\ti\pdk_OMAPL138_1_01_00_02\packages\ti\drv\exampleProjects\MCBSP_MasterExampleProject.
I'm using OMAP L138 LCDK. The digital output of a custom board which contains an ADS1602 Analog to Digital converter is connected to the J15.23 extension of the OMAP L138 LCDK. This custom boards converts some analog signals to digital and then sends them to the OMAP L138 Board. The OMAP L138 LCDK receives this digital data via MCBSP module. As far as I know, by default, the MCBSP_MasterExampleProject saves the received data on the memory, right?
First, I would like to know that this received data is saved in which part of the memory.
Second, I would like to know how can I save this received data (which is on the memory) on an Excel or Matlab file (any other similar format is also acceptable).
Thank you so much in advance :)