Hi there, I am trying to run the NAND example on the OMAPL138 LCDK and its working. However, if I re-run the example it complains that the block is bad ans can't continue.
I have try to go through the steps the example is doing and there is only one place when the sw will mark the block as bad. And that is only if the erase block function fails to complete.
With adding breakpoints and removing the function call to mark the block as bad .. it still fails when I try to re-run the example and write to the same location.
Should I need to do a random write/ read, before using PageWrite command for same block and page?
I am using -> OMAPL138_StarterWare_1_10_04_01
Thanks in advance.
Regards
Mitesh