Hello,
I am using an OMAP L-138 DSP+ARM9 development kit to test an USB camera. On the first time that i have connected the camera to this development kit, i noticed that the v4l2 drivers weren't present. So, i started to search over the internet, and i have found that to activate this video drivers, it was needed to rebuild the kernel and activate some options on a config menu. I was able to build the kernel and activate the the options on the config menu, but when i load the kernel image to the board, it got stuck on the message 'Starting Kernel...' of the serial terminal. Maybe i did a lot of error on the way long, so i am describing my procedure bellow.
I started to follow this guide to rebuild the kernel:
http://processors.wiki.ti.com/index.php/Building_03.22_PSP_release_Components_for_OMAP-L138#Basic_Configuration_of_the_Kernel
and i have activated the following options in the config menu:
System Type ---> TI DaVinci Implementations ---> [*] TI DA850/OMAP-L138/AM18xx Reference Platform Select peripherals connected to expander on UI board (Video Port Interface) ---> Device Drivers ---> <*> Multimedia support ---> <*> Video For Linux [*] Video capture adapters ---> [*] V4L platform devices ---> <*> DM646x/DA850/OMAPL138 EVM Video Display <*> DM646x/DA850/OMAPL138 EVM Video Capture -*- DaVinci VPIF Driver [ ] Autoselect pertinent encoders/decoders and other helper chips Encoders/decoders and other helper chips ---> <*> Texas Instruments TVP514x video decoder -*- ADV7343 video encoder -*- THS7303 Video Amplifier
While trying to compile the kernel i got this erro:
In order to avoid this error , i have comment the 3 responsible lines on kernel/timeconst.pl file, and it worked:
---At the end of the file---
} else { $hz += 0; # Force to number if ($hz < 1) { die "Usage: $0 HZ\n"; } @val = @{$canned_values{$hz}}; #if (!defined(@val)) { # @val = compute_values($hz); #} output($hz, @val); }
After editing the file, and repeating the command to build the kernel image, i was able to generate the image as expected, here are the .config file
# # Automatically generated make config: don't edit # Linux kernel version: 2.6.33-rc4 # Mon Oct 17 08:19:30 2016 # CONFIG_ARM=y CONFIG_SYS_SUPPORTS_APM_EMULATION=y CONFIG_GENERIC_GPIO=y CONFIG_GENERIC_TIME=y CONFIG_GENERIC_CLOCKEVENTS=y CONFIG_GENERIC_HARDIRQS=y CONFIG_STACKTRACE_SUPPORT=y CONFIG_HAVE_LATENCYTOP_SUPPORT=y CONFIG_LOCKDEP_SUPPORT=y CONFIG_TRACE_IRQFLAGS_SUPPORT=y CONFIG_HARDIRQS_SW_RESEND=y CONFIG_GENERIC_IRQ_PROBE=y CONFIG_RWSEM_GENERIC_SPINLOCK=y CONFIG_ARCH_HAS_CPUFREQ=y CONFIG_GENERIC_HWEIGHT=y CONFIG_GENERIC_CALIBRATE_DELAY=y CONFIG_ZONE_DMA=y CONFIG_GENERIC_HARDIRQS_NO__DO_IRQ=y CONFIG_VECTORS_BASE=0xffff0000 CONFIG_DEFCONFIG_LIST="/lib/modules/$UNAME_RELEASE/.config" CONFIG_CONSTRUCTORS=y # # General setup # CONFIG_EXPERIMENTAL=y CONFIG_BROKEN_ON_SMP=y CONFIG_LOCK_KERNEL=y CONFIG_INIT_ENV_ARG_LIMIT=32 CONFIG_LOCALVERSION="" # CONFIG_LOCALVERSION_AUTO is not set CONFIG_HAVE_KERNEL_GZIP=y CONFIG_HAVE_KERNEL_LZO=y CONFIG_KERNEL_GZIP=y # CONFIG_KERNEL_BZIP2 is not set # CONFIG_KERNEL_LZMA is not set # CONFIG_KERNEL_LZO is not set CONFIG_SWAP=y CONFIG_SYSVIPC=y CONFIG_SYSVIPC_SYSCTL=y CONFIG_POSIX_MQUEUE=y CONFIG_POSIX_MQUEUE_SYSCTL=y # CONFIG_BSD_PROCESS_ACCT is not set # CONFIG_TASKSTATS is not set # CONFIG_AUDIT is not set # # RCU Subsystem # CONFIG_TREE_RCU=y # CONFIG_TREE_PREEMPT_RCU is not set # CONFIG_TINY_RCU is not set # CONFIG_RCU_TRACE is not set CONFIG_RCU_FANOUT=32 # CONFIG_RCU_FANOUT_EXACT is not set # CONFIG_TREE_RCU_TRACE is not set CONFIG_IKCONFIG=y CONFIG_IKCONFIG_PROC=y CONFIG_LOG_BUF_SHIFT=14 CONFIG_GROUP_SCHED=y CONFIG_FAIR_GROUP_SCHED=y # CONFIG_RT_GROUP_SCHED is not set CONFIG_USER_SCHED=y # CONFIG_CGROUP_SCHED is not set # CONFIG_CGROUPS is not set # CONFIG_SYSFS_DEPRECATED_V2 is not set # CONFIG_RELAY is not set # CONFIG_NAMESPACES is not set CONFIG_BLK_DEV_INITRD=y CONFIG_INITRAMFS_SOURCE="" CONFIG_RD_GZIP=y # CONFIG_RD_BZIP2 is not set # CONFIG_RD_LZMA is not set # CONFIG_RD_LZO is not set CONFIG_CC_OPTIMIZE_FOR_SIZE=y CONFIG_SYSCTL=y CONFIG_ANON_INODES=y CONFIG_EMBEDDED=y CONFIG_UID16=y CONFIG_SYSCTL_SYSCALL=y CONFIG_KALLSYMS=y # CONFIG_KALLSYMS_EXTRA_PASS is not set CONFIG_HOTPLUG=y CONFIG_PRINTK=y CONFIG_BUG=y CONFIG_ELF_CORE=y CONFIG_BASE_FULL=y CONFIG_FUTEX=y CONFIG_EPOLL=y CONFIG_SIGNALFD=y CONFIG_TIMERFD=y CONFIG_EVENTFD=y CONFIG_SHMEM=y CONFIG_AIO=y # # Kernel Performance Events And Counters # CONFIG_VM_EVENT_COUNTERS=y CONFIG_SLUB_DEBUG=y CONFIG_COMPAT_BRK=y # CONFIG_SLAB is not set CONFIG_SLUB=y # CONFIG_SLOB is not set # CONFIG_PROFILING is not set CONFIG_HAVE_OPROFILE=y # CONFIG_KPROBES is not set CONFIG_HAVE_KPROBES=y CONFIG_HAVE_KRETPROBES=y CONFIG_HAVE_CLK=y # # GCOV-based kernel profiling # # CONFIG_GCOV_KERNEL is not set # CONFIG_SLOW_WORK is not set CONFIG_HAVE_GENERIC_DMA_COHERENT=y CONFIG_SLABINFO=y CONFIG_RT_MUTEXES=y CONFIG_BASE_SMALL=0 CONFIG_MODULES=y # CONFIG_MODULE_FORCE_LOAD is not set CONFIG_MODULE_UNLOAD=y CONFIG_MODULE_FORCE_UNLOAD=y CONFIG_MODVERSIONS=y # CONFIG_MODULE_SRCVERSION_ALL is not set CONFIG_BLOCK=y CONFIG_LBDAF=y # CONFIG_BLK_DEV_BSG is not set # CONFIG_BLK_DEV_INTEGRITY is not set # # IO Schedulers # CONFIG_IOSCHED_NOOP=y # CONFIG_IOSCHED_DEADLINE is not set # CONFIG_IOSCHED_CFQ is not set # CONFIG_DEFAULT_DEADLINE is not set # CONFIG_DEFAULT_CFQ is not set CONFIG_DEFAULT_NOOP=y CONFIG_DEFAULT_IOSCHED="noop" # CONFIG_INLINE_SPIN_TRYLOCK is not set # CONFIG_INLINE_SPIN_TRYLOCK_BH is not set # CONFIG_INLINE_SPIN_LOCK is not set # CONFIG_INLINE_SPIN_LOCK_BH is not set # CONFIG_INLINE_SPIN_LOCK_IRQ is not set # CONFIG_INLINE_SPIN_LOCK_IRQSAVE is not set # CONFIG_INLINE_SPIN_UNLOCK is not set # CONFIG_INLINE_SPIN_UNLOCK_BH is not set # CONFIG_INLINE_SPIN_UNLOCK_IRQ is not set # CONFIG_INLINE_SPIN_UNLOCK_IRQRESTORE is not set # CONFIG_INLINE_READ_TRYLOCK is not set # CONFIG_INLINE_READ_LOCK is not set # CONFIG_INLINE_READ_LOCK_BH is not set # CONFIG_INLINE_READ_LOCK_IRQ is not set # CONFIG_INLINE_READ_LOCK_IRQSAVE is not set # CONFIG_INLINE_READ_UNLOCK is not set # CONFIG_INLINE_READ_UNLOCK_BH is not set # CONFIG_INLINE_READ_UNLOCK_IRQ is not set # CONFIG_INLINE_READ_UNLOCK_IRQRESTORE is not set # CONFIG_INLINE_WRITE_TRYLOCK is not set # CONFIG_INLINE_WRITE_LOCK is not set # CONFIG_INLINE_WRITE_LOCK_BH is not set # CONFIG_INLINE_WRITE_LOCK_IRQ is not set # CONFIG_INLINE_WRITE_LOCK_IRQSAVE is not set # CONFIG_INLINE_WRITE_UNLOCK is not set # CONFIG_INLINE_WRITE_UNLOCK_BH is not set # CONFIG_INLINE_WRITE_UNLOCK_IRQ is not set # CONFIG_INLINE_WRITE_UNLOCK_IRQRESTORE is not set # CONFIG_MUTEX_SPIN_ON_OWNER is not set CONFIG_FREEZER=y # # System Type # CONFIG_MMU=y # CONFIG_ARCH_AAEC2000 is not set # CONFIG_ARCH_INTEGRATOR is not set # CONFIG_ARCH_REALVIEW is not set # CONFIG_ARCH_VERSATILE is not set # CONFIG_ARCH_AT91 is not set # CONFIG_ARCH_CLPS711X is not set # CONFIG_ARCH_GEMINI is not set # CONFIG_ARCH_EBSA110 is not set # CONFIG_ARCH_EP93XX is not set # CONFIG_ARCH_FOOTBRIDGE is not set # CONFIG_ARCH_MXC is not set # CONFIG_ARCH_STMP3XXX is not set # CONFIG_ARCH_NETX is not set # CONFIG_ARCH_H720X is not set # CONFIG_ARCH_NOMADIK is not set # CONFIG_ARCH_IOP13XX is not set # CONFIG_ARCH_IOP32X is not set # CONFIG_ARCH_IOP33X is not set # CONFIG_ARCH_IXP23XX is not set # CONFIG_ARCH_IXP2000 is not set # CONFIG_ARCH_IXP4XX is not set # CONFIG_ARCH_L7200 is not set # CONFIG_ARCH_DOVE is not set # CONFIG_ARCH_KIRKWOOD is not set # CONFIG_ARCH_LOKI is not set # CONFIG_ARCH_MV78XX0 is not set # CONFIG_ARCH_ORION5X is not set # CONFIG_ARCH_MMP is not set # CONFIG_ARCH_KS8695 is not set # CONFIG_ARCH_NS9XXX is not set # CONFIG_ARCH_W90X900 is not set # CONFIG_ARCH_PNX4008 is not set # CONFIG_ARCH_PXA is not set # CONFIG_ARCH_MSM is not set # CONFIG_ARCH_RPC is not set # CONFIG_ARCH_SA1100 is not set # CONFIG_ARCH_S3C2410 is not set # CONFIG_ARCH_S3C64XX is not set # CONFIG_ARCH_S5PC1XX is not set # CONFIG_ARCH_SHARK is not set # CONFIG_ARCH_LH7A40X is not set # CONFIG_ARCH_U300 is not set CONFIG_ARCH_DAVINCI=y # CONFIG_ARCH_OMAP is not set # CONFIG_ARCH_BCMRING is not set # CONFIG_ARCH_U8500 is not set CONFIG_CP_INTC=y # # TI DaVinci Implementations # # # DaVinci Core Type # # CONFIG_ARCH_DAVINCI_DM644x is not set # CONFIG_ARCH_DAVINCI_DM355 is not set # CONFIG_ARCH_DAVINCI_DM646x is not set # CONFIG_ARCH_DAVINCI_DA830 is not set CONFIG_ARCH_DAVINCI_DA850=y # CONFIG_DA8XX_MAX_SPEED_300 is not set # CONFIG_DA8XX_MAX_SPEED_372 is not set # CONFIG_DA8XX_MAX_SPEED_408 is not set CONFIG_DA8XX_MAX_SPEED_456=y CONFIG_ARCH_DAVINCI_DA8XX=y # CONFIG_ARCH_DAVINCI_DM365 is not set # # DaVinci Board Type # CONFIG_MACH_DAVINCI_DA850_EVM=y CONFIG_DA850_UI_NONE=y # CONFIG_DA850_UI_RMII is not set # CONFIG_DA850_UI_CLCD is not set # CONFIG_DA850_UI_VIDEO_PORT is not set CONFIG_DAVINCI_MUX=y # CONFIG_DAVINCI_MUX_DEBUG is not set # CONFIG_DAVINCI_MUX_WARNINGS is not set CONFIG_DAVINCI_RESET_CLOCKS=y # CONFIG_DAVINCI_MCBSP is not set # # Processor Type # CONFIG_CPU_ARM926T=y CONFIG_CPU_32v5=y CONFIG_CPU_ABRT_EV5TJ=y CONFIG_CPU_PABRT_LEGACY=y CONFIG_CPU_CACHE_VIVT=y CONFIG_CPU_COPY_V4WB=y CONFIG_CPU_TLB_V4WBI=y CONFIG_CPU_CP15=y CONFIG_CPU_CP15_MMU=y # # Processor Features # CONFIG_ARM_THUMB=y # CONFIG_CPU_ICACHE_DISABLE is not set # CONFIG_CPU_DCACHE_DISABLE is not set # CONFIG_CPU_DCACHE_WRITETHROUGH is not set # CONFIG_CPU_CACHE_ROUND_ROBIN is not set CONFIG_ARM_L1_CACHE_SHIFT=5 CONFIG_COMMON_CLKDEV=y # # Bus support # # CONFIG_PCI_SYSCALL is not set # CONFIG_ARCH_SUPPORTS_MSI is not set # CONFIG_PCCARD is not set # # Kernel Features # CONFIG_TICK_ONESHOT=y CONFIG_NO_HZ=y CONFIG_HIGH_RES_TIMERS=y CONFIG_GENERIC_CLOCKEVENTS_BUILD=y CONFIG_VMSPLIT_3G=y # CONFIG_VMSPLIT_2G is not set # CONFIG_VMSPLIT_1G is not set CONFIG_PAGE_OFFSET=0xC0000000 # CONFIG_PREEMPT_NONE is not set # CONFIG_PREEMPT_VOLUNTARY is not set CONFIG_PREEMPT=y CONFIG_HZ=100 CONFIG_AEABI=y # CONFIG_OABI_COMPAT is not set CONFIG_ARCH_HAS_HOLES_MEMORYMODEL=y # CONFIG_ARCH_SPARSEMEM_DEFAULT is not set # CONFIG_ARCH_SELECT_MEMORY_MODEL is not set # CONFIG_HIGHMEM is not set CONFIG_SELECT_MEMORY_MODEL=y CONFIG_FLATMEM_MANUAL=y # CONFIG_DISCONTIGMEM_MANUAL is not set # CONFIG_SPARSEMEM_MANUAL is not set CONFIG_FLATMEM=y CONFIG_FLAT_NODE_MEM_MAP=y CONFIG_PAGEFLAGS_EXTENDED=y CONFIG_SPLIT_PTLOCK_CPUS=999999 # CONFIG_PHYS_ADDR_T_64BIT is not set CONFIG_ZONE_DMA_FLAG=1 CONFIG_BOUNCE=y CONFIG_VIRT_TO_BUS=y # CONFIG_KSM is not set CONFIG_DEFAULT_MMAP_MIN_ADDR=4096 CONFIG_LEDS=y # CONFIG_LEDS_CPU is not set CONFIG_ALIGNMENT_TRAP=y # CONFIG_UACCESS_WITH_MEMCPY is not set # # Boot options # CONFIG_ZBOOT_ROM_TEXT=0x0 CONFIG_ZBOOT_ROM_BSS=0x0 CONFIG_CMDLINE="" # CONFIG_XIP_KERNEL is not set # CONFIG_KEXEC is not set # # CPU Power Management # CONFIG_CPU_FREQ=y CONFIG_CPU_FREQ_TABLE=y # CONFIG_CPU_FREQ_DEBUG is not set CONFIG_CPU_FREQ_STAT=y # CONFIG_CPU_FREQ_STAT_DETAILS is not set # CONFIG_CPU_FREQ_DEFAULT_GOV_PERFORMANCE is not set # CONFIG_CPU_FREQ_DEFAULT_GOV_POWERSAVE is not set CONFIG_CPU_FREQ_DEFAULT_GOV_USERSPACE=y # CONFIG_CPU_FREQ_DEFAULT_GOV_ONDEMAND is not set # CONFIG_CPU_FREQ_DEFAULT_GOV_CONSERVATIVE is not set CONFIG_CPU_FREQ_GOV_PERFORMANCE=y CONFIG_CPU_FREQ_GOV_POWERSAVE=y CONFIG_CPU_FREQ_GOV_USERSPACE=y CONFIG_CPU_FREQ_GOV_ONDEMAND=y CONFIG_CPU_FREQ_GOV_CONSERVATIVE=y CONFIG_CPU_IDLE=y CONFIG_CPU_IDLE_GOV_LADDER=y CONFIG_CPU_IDLE_GOV_MENU=y # # Floating point emulation # # # At least one emulation must be selected # # CONFIG_VFP is not set # # Userspace binary formats # CONFIG_BINFMT_ELF=y # CONFIG_CORE_DUMP_DEFAULT_ELF_HEADERS is not set CONFIG_HAVE_AOUT=y # CONFIG_BINFMT_AOUT is not set # CONFIG_BINFMT_MISC is not set # # Power management options # CONFIG_PM=y # CONFIG_PM_DEBUG is not set CONFIG_PM_SLEEP=y CONFIG_SUSPEND=y CONFIG_SUSPEND_FREEZER=y # CONFIG_APM_EMULATION is not set # CONFIG_PM_RUNTIME is not set CONFIG_ARCH_SUSPEND_POSSIBLE=y CONFIG_NET=y # # Networking options # CONFIG_PACKET=y # CONFIG_PACKET_MMAP is not set CONFIG_UNIX=y CONFIG_XFRM=y # CONFIG_XFRM_USER is not set # CONFIG_XFRM_SUB_POLICY is not set # CONFIG_XFRM_MIGRATE is not set # CONFIG_XFRM_STATISTICS is not set # CONFIG_NET_KEY is not set CONFIG_INET=y # CONFIG_IP_MULTICAST is not set # CONFIG_IP_ADVANCED_ROUTER is not set CONFIG_IP_FIB_HASH=y CONFIG_IP_PNP=y CONFIG_IP_PNP_DHCP=y # CONFIG_IP_PNP_BOOTP is not set # CONFIG_IP_PNP_RARP is not set # CONFIG_NET_IPIP is not set # CONFIG_NET_IPGRE is not set # CONFIG_ARPD is not set # CONFIG_SYN_COOKIES is not set # CONFIG_INET_AH is not set # CONFIG_INET_ESP is not set # CONFIG_INET_IPCOMP is not set # CONFIG_INET_XFRM_TUNNEL is not set CONFIG_INET_TUNNEL=m CONFIG_INET_XFRM_MODE_TRANSPORT=y CONFIG_INET_XFRM_MODE_TUNNEL=y CONFIG_INET_XFRM_MODE_BEET=y # CONFIG_INET_LRO is not set CONFIG_INET_DIAG=y CONFIG_INET_TCP_DIAG=y # CONFIG_TCP_CONG_ADVANCED is not set CONFIG_TCP_CONG_CUBIC=y CONFIG_DEFAULT_TCP_CONG="cubic" # CONFIG_TCP_MD5SIG is not set CONFIG_IPV6=m # CONFIG_IPV6_PRIVACY is not set # CONFIG_IPV6_ROUTER_PREF is not set # CONFIG_IPV6_OPTIMISTIC_DAD is not set # CONFIG_INET6_AH is not set # CONFIG_INET6_ESP is not set # CONFIG_INET6_IPCOMP is not set # CONFIG_IPV6_MIP6 is not set # CONFIG_INET6_XFRM_TUNNEL is not set # CONFIG_INET6_TUNNEL is not set CONFIG_INET6_XFRM_MODE_TRANSPORT=m CONFIG_INET6_XFRM_MODE_TUNNEL=m CONFIG_INET6_XFRM_MODE_BEET=m # CONFIG_INET6_XFRM_MODE_ROUTEOPTIMIZATION is not set CONFIG_IPV6_SIT=m # CONFIG_IPV6_SIT_6RD is not set CONFIG_IPV6_NDISC_NODETYPE=y # CONFIG_IPV6_TUNNEL is not set # CONFIG_IPV6_MULTIPLE_TABLES is not set # CONFIG_IPV6_MROUTE is not set # CONFIG_NETWORK_SECMARK is not set CONFIG_NETFILTER=y # CONFIG_NETFILTER_DEBUG is not set CONFIG_NETFILTER_ADVANCED=y # # Core Netfilter Configuration # # CONFIG_NETFILTER_NETLINK_QUEUE is not set # CONFIG_NETFILTER_NETLINK_LOG is not set # CONFIG_NF_CONNTRACK is not set # CONFIG_NETFILTER_XTABLES is not set # CONFIG_IP_VS is not set # # IP: Netfilter Configuration # # CONFIG_NF_DEFRAG_IPV4 is not set # CONFIG_IP_NF_QUEUE is not set # CONFIG_IP_NF_IPTABLES is not set # CONFIG_IP_NF_ARPTABLES is not set # # IPv6: Netfilter Configuration # # CONFIG_IP6_NF_QUEUE is not set # CONFIG_IP6_NF_IPTABLES is not set # CONFIG_IP_DCCP is not set # CONFIG_IP_SCTP is not set # CONFIG_RDS is not set # CONFIG_TIPC is not set # CONFIG_ATM is not set # CONFIG_BRIDGE is not set # CONFIG_NET_DSA is not set # CONFIG_VLAN_8021Q is not set # CONFIG_DECNET is not set # CONFIG_LLC2 is not set # CONFIG_IPX is not set # CONFIG_ATALK is not set # CONFIG_X25 is not set # CONFIG_LAPB is not set # CONFIG_ECONET is not set # CONFIG_WAN_ROUTER is not set # CONFIG_PHONET is not set # CONFIG_IEEE802154 is not set # CONFIG_NET_SCHED is not set # CONFIG_DCB is not set # # Network testing # # CONFIG_NET_PKTGEN is not set # CONFIG_HAMRADIO is not set # CONFIG_CAN is not set # CONFIG_IRDA is not set # CONFIG_BT is not set # CONFIG_AF_RXRPC is not set CONFIG_WIRELESS=y # CONFIG_CFG80211 is not set # CONFIG_LIB80211 is not set # # CFG80211 needs to be enabled for MAC80211 # # CONFIG_WIMAX is not set # CONFIG_RFKILL is not set # CONFIG_NET_9P is not set # # Device Drivers # # # Generic Driver Options # CONFIG_UEVENT_HELPER_PATH="/sbin/hotplug" # CONFIG_DEVTMPFS is not set CONFIG_STANDALONE=y CONFIG_PREVENT_FIRMWARE_BUILD=y # CONFIG_FW_LOADER is not set # CONFIG_SYS_HYPERVISOR is not set # CONFIG_CONNECTOR is not set CONFIG_MTD=y # CONFIG_MTD_DEBUG is not set # CONFIG_MTD_TESTS is not set # CONFIG_MTD_CONCAT is not set CONFIG_MTD_PARTITIONS=y # CONFIG_MTD_REDBOOT_PARTS is not set # CONFIG_MTD_CMDLINE_PARTS is not set # CONFIG_MTD_AFS_PARTS is not set # CONFIG_MTD_AR7_PARTS is not set # # User Modules And Translation Layers # CONFIG_MTD_CHAR=y CONFIG_MTD_BLKDEVS=y CONFIG_MTD_BLOCK=y # CONFIG_FTL is not set # CONFIG_NFTL is not set # CONFIG_INFTL is not set # CONFIG_RFD_FTL is not set # CONFIG_SSFDC is not set # CONFIG_MTD_OOPS is not set # # RAM/ROM/Flash chip drivers # # CONFIG_MTD_CFI is not set # CONFIG_MTD_JEDECPROBE is not set CONFIG_MTD_MAP_BANK_WIDTH_1=y CONFIG_MTD_MAP_BANK_WIDTH_2=y CONFIG_MTD_MAP_BANK_WIDTH_4=y # CONFIG_MTD_MAP_BANK_WIDTH_8 is not set # CONFIG_MTD_MAP_BANK_WIDTH_16 is not set # CONFIG_MTD_MAP_BANK_WIDTH_32 is not set CONFIG_MTD_CFI_I1=y CONFIG_MTD_CFI_I2=y # CONFIG_MTD_CFI_I4 is not set # CONFIG_MTD_CFI_I8 is not set # CONFIG_MTD_RAM is not set # CONFIG_MTD_ROM is not set # CONFIG_MTD_ABSENT is not set # # Mapping drivers for chip access # # CONFIG_MTD_COMPLEX_MAPPINGS is not set # CONFIG_MTD_PLATRAM is not set # # Self-contained MTD device drivers # # CONFIG_MTD_DATAFLASH is not set CONFIG_MTD_M25P80=y CONFIG_M25PXX_USE_FAST_READ=y # CONFIG_MTD_SST25L is not set # CONFIG_MTD_SLRAM is not set # CONFIG_MTD_PHRAM is not set # CONFIG_MTD_MTDRAM is not set # CONFIG_MTD_BLOCK2MTD is not set # # Disk-On-Chip Device Drivers # # CONFIG_MTD_DOC2000 is not set # CONFIG_MTD_DOC2001 is not set # CONFIG_MTD_DOC2001PLUS is not set # CONFIG_MTD_NAND is not set # CONFIG_MTD_ONENAND is not set # # LPDDR flash memory drivers # # CONFIG_MTD_LPDDR is not set # # UBI - Unsorted block images # # CONFIG_MTD_UBI is not set # CONFIG_PARPORT is not set CONFIG_BLK_DEV=y # CONFIG_BLK_DEV_COW_COMMON is not set CONFIG_BLK_DEV_LOOP=m # CONFIG_BLK_DEV_CRYPTOLOOP is not set # # DRBD disabled because PROC_FS, INET or CONNECTOR not selected # # CONFIG_BLK_DEV_NBD is not set # CONFIG_BLK_DEV_UB is not set CONFIG_BLK_DEV_RAM=y CONFIG_BLK_DEV_RAM_COUNT=1 CONFIG_BLK_DEV_RAM_SIZE=32768 # CONFIG_BLK_DEV_XIP is not set # CONFIG_CDROM_PKTCDVD is not set # CONFIG_ATA_OVER_ETH is not set # CONFIG_MG_DISK is not set CONFIG_MISC_DEVICES=y # CONFIG_AD525X_DPOT is not set # CONFIG_ICS932S401 is not set # CONFIG_ENCLOSURE_SERVICES is not set # CONFIG_ISL29003 is not set # CONFIG_DS1682 is not set # CONFIG_TI_DAC7512 is not set # CONFIG_C2PORT is not set # # EEPROM support # CONFIG_EEPROM_AT24=y # CONFIG_EEPROM_AT25 is not set # CONFIG_EEPROM_LEGACY is not set # CONFIG_EEPROM_MAX6875 is not set # CONFIG_EEPROM_93CX6 is not set # CONFIG_IWMC3200TOP is not set CONFIG_HAVE_IDE=y # CONFIG_IDE is not set # # SCSI device support # # CONFIG_RAID_ATTRS is not set CONFIG_SCSI=y CONFIG_SCSI_DMA=y # CONFIG_SCSI_TGT is not set # CONFIG_SCSI_NETLINK is not set CONFIG_SCSI_PROC_FS=y # # SCSI support type (disk, tape, CD-ROM) # CONFIG_BLK_DEV_SD=y # CONFIG_CHR_DEV_ST is not set # CONFIG_CHR_DEV_OSST is not set # CONFIG_BLK_DEV_SR is not set CONFIG_CHR_DEV_SG=y # CONFIG_CHR_DEV_SCH is not set # CONFIG_SCSI_MULTI_LUN is not set # CONFIG_SCSI_CONSTANTS is not set # CONFIG_SCSI_LOGGING is not set # CONFIG_SCSI_SCAN_ASYNC is not set CONFIG_SCSI_WAIT_SCAN=m # # SCSI Transports # # CONFIG_SCSI_SPI_ATTRS is not set # CONFIG_SCSI_FC_ATTRS is not set # CONFIG_SCSI_ISCSI_ATTRS is not set # CONFIG_SCSI_SAS_LIBSAS is not set # CONFIG_SCSI_SRP_ATTRS is not set CONFIG_SCSI_LOWLEVEL=y # CONFIG_ISCSI_TCP is not set # CONFIG_LIBFC is not set # CONFIG_LIBFCOE is not set # CONFIG_SCSI_DEBUG is not set # CONFIG_SCSI_DH is not set # CONFIG_SCSI_OSD_INITIATOR is not set CONFIG_ATA=y # CONFIG_ATA_NONSTANDARD is not set CONFIG_ATA_VERBOSE_ERROR=y CONFIG_SATA_PMP=y CONFIG_SATA_AHCI=y # CONFIG_ATA_SFF is not set # CONFIG_MD is not set CONFIG_NETDEVICES=y # CONFIG_DUMMY is not set # CONFIG_BONDING is not set # CONFIG_MACVLAN is not set # CONFIG_EQUALIZER is not set # CONFIG_TUN is not set # CONFIG_VETH is not set CONFIG_PHYLIB=y # # MII PHY device drivers # # CONFIG_MARVELL_PHY is not set # CONFIG_DAVICOM_PHY is not set # CONFIG_QSEMI_PHY is not set CONFIG_LXT_PHY=y # CONFIG_CICADA_PHY is not set # CONFIG_VITESSE_PHY is not set CONFIG_SMSC_PHY=y # CONFIG_BROADCOM_PHY is not set # CONFIG_ICPLUS_PHY is not set # CONFIG_REALTEK_PHY is not set # CONFIG_NATIONAL_PHY is not set # CONFIG_STE10XP is not set CONFIG_LSI_ET1011C_PHY=y # CONFIG_FIXED_PHY is not set # CONFIG_MDIO_BITBANG is not set CONFIG_NET_ETHERNET=y CONFIG_MII=y # CONFIG_AX88796 is not set # CONFIG_SMC91X is not set CONFIG_TI_DAVINCI_EMAC=y # CONFIG_DM9000 is not set # CONFIG_ENC28J60 is not set # CONFIG_ETHOC is not set # CONFIG_SMC911X is not set # CONFIG_SMSC911X is not set # CONFIG_DNET is not set # CONFIG_IBM_NEW_EMAC_ZMII is not set # CONFIG_IBM_NEW_EMAC_RGMII is not set # CONFIG_IBM_NEW_EMAC_TAH is not set # CONFIG_IBM_NEW_EMAC_EMAC4 is not set # CONFIG_IBM_NEW_EMAC_NO_FLOW_CTRL is not set # CONFIG_IBM_NEW_EMAC_MAL_CLR_ICINTSTAT is not set # CONFIG_IBM_NEW_EMAC_MAL_COMMON_ERR is not set # CONFIG_B44 is not set # CONFIG_KS8842 is not set # CONFIG_KS8851 is not set # CONFIG_KS8851_MLL is not set # CONFIG_NETDEV_1000 is not set # CONFIG_NETDEV_10000 is not set CONFIG_WLAN=y # CONFIG_USB_ZD1201 is not set # CONFIG_HOSTAP is not set # # Enable WiMAX (Networking options) to see the WiMAX drivers # # # USB Network Adapters # # CONFIG_USB_CATC is not set # CONFIG_USB_KAWETH is not set # CONFIG_USB_PEGASUS is not set # CONFIG_USB_RTL8150 is not set # CONFIG_USB_USBNET is not set # CONFIG_WAN is not set # CONFIG_PPP is not set # CONFIG_SLIP is not set CONFIG_NETCONSOLE=y # CONFIG_NETCONSOLE_DYNAMIC is not set CONFIG_NETPOLL=y CONFIG_NETPOLL_TRAP=y CONFIG_NET_POLL_CONTROLLER=y # CONFIG_ISDN is not set # CONFIG_PHONE is not set # # Input device support # CONFIG_INPUT=y # CONFIG_INPUT_FF_MEMLESS is not set # CONFIG_INPUT_POLLDEV is not set # CONFIG_INPUT_SPARSEKMAP is not set # # Userland interfaces # # CONFIG_INPUT_MOUSEDEV is not set # CONFIG_INPUT_JOYDEV is not set CONFIG_INPUT_EVDEV=y # CONFIG_INPUT_EVBUG is not set # # Input Device Drivers # CONFIG_INPUT_KEYBOARD=y # CONFIG_KEYBOARD_ADP5588 is not set CONFIG_KEYBOARD_ATKBD=m # CONFIG_QT2160 is not set # CONFIG_KEYBOARD_LKKBD is not set CONFIG_KEYBOARD_GPIO=y # CONFIG_KEYBOARD_MATRIX is not set # CONFIG_KEYBOARD_MAX7359 is not set # CONFIG_KEYBOARD_NEWTON is not set # CONFIG_KEYBOARD_OPENCORES is not set # CONFIG_KEYBOARD_STOWAWAY is not set # CONFIG_KEYBOARD_SUNKBD is not set CONFIG_KEYBOARD_XTKBD=m # CONFIG_INPUT_MOUSE is not set # CONFIG_INPUT_JOYSTICK is not set # CONFIG_INPUT_TABLET is not set CONFIG_INPUT_TOUCHSCREEN=y # CONFIG_TOUCHSCREEN_ADS7846 is not set # CONFIG_TOUCHSCREEN_AD7877 is not set # CONFIG_TOUCHSCREEN_AD7879_I2C is not set # CONFIG_TOUCHSCREEN_AD7879_SPI is not set # CONFIG_TOUCHSCREEN_AD7879 is not set # CONFIG_TOUCHSCREEN_DYNAPRO is not set # CONFIG_TOUCHSCREEN_EETI is not set # CONFIG_TOUCHSCREEN_FUJITSU is not set # CONFIG_TOUCHSCREEN_GUNZE is not set # CONFIG_TOUCHSCREEN_ELO is not set # CONFIG_TOUCHSCREEN_WACOM_W8001 is not set # CONFIG_TOUCHSCREEN_MCS5000 is not set # CONFIG_TOUCHSCREEN_MTOUCH is not set # CONFIG_TOUCHSCREEN_INEXIO is not set # CONFIG_TOUCHSCREEN_MK712 is not set # CONFIG_TOUCHSCREEN_PENMOUNT is not set # CONFIG_TOUCHSCREEN_TOUCHRIGHT is not set # CONFIG_TOUCHSCREEN_TOUCHWIN is not set # CONFIG_TOUCHSCREEN_USB_COMPOSITE is not set # CONFIG_TOUCHSCREEN_TOUCHIT213 is not set # CONFIG_TOUCHSCREEN_TSC2007 is not set # CONFIG_TOUCHSCREEN_TSC2004 is not set # CONFIG_TOUCHSCREEN_W90X900 is not set CONFIG_TOUCHSCREEN_TPS6507X=y # CONFIG_INPUT_MISC is not set # # Hardware I/O ports # CONFIG_SERIO=y CONFIG_SERIO_SERPORT=y CONFIG_SERIO_LIBPS2=y # CONFIG_SERIO_RAW is not set # CONFIG_SERIO_ALTERA_PS2 is not set # CONFIG_GAMEPORT is not set # # Character devices # CONFIG_VT=y CONFIG_CONSOLE_TRANSLATIONS=y # CONFIG_VT_CONSOLE is not set CONFIG_HW_CONSOLE=y # CONFIG_VT_HW_CONSOLE_BINDING is not set CONFIG_DEVKMEM=y # CONFIG_SERIAL_NONSTANDARD is not set # # Serial drivers # CONFIG_SERIAL_8250=y CONFIG_SERIAL_8250_CONSOLE=y CONFIG_SERIAL_8250_NR_UARTS=3 CONFIG_SERIAL_8250_RUNTIME_UARTS=3 # CONFIG_SERIAL_8250_EXTENDED is not set # # Non-8250 serial port support # # CONFIG_SERIAL_MAX3100 is not set CONFIG_SERIAL_CORE=y CONFIG_SERIAL_CORE_CONSOLE=y CONFIG_UNIX98_PTYS=y # CONFIG_DEVPTS_MULTIPLE_INSTANCES is not set CONFIG_LEGACY_PTYS=y CONFIG_LEGACY_PTY_COUNT=8 # CONFIG_IPMI_HANDLER is not set CONFIG_HW_RANDOM=m # CONFIG_HW_RANDOM_TIMERIOMEM is not set # CONFIG_R3964 is not set # CONFIG_RAW_DRIVER is not set # CONFIG_TCG_TPM is not set CONFIG_I2C=y CONFIG_I2C_BOARDINFO=y CONFIG_I2C_COMPAT=y CONFIG_I2C_CHARDEV=y CONFIG_I2C_HELPER_AUTO=y CONFIG_I2C_ALGOBIT=y # # I2C Hardware Bus support # # # I2C system bus drivers (mostly embedded / system-on-chip) # CONFIG_I2C_DAVINCI=y # CONFIG_I2C_DESIGNWARE is not set CONFIG_I2C_GPIO=y # CONFIG_I2C_OCORES is not set # CONFIG_I2C_SIMTEC is not set # # External I2C/SMBus adapter drivers # # CONFIG_I2C_PARPORT_LIGHT is not set # CONFIG_I2C_TAOS_EVM is not set # CONFIG_I2C_TINY_USB is not set # # Other I2C/SMBus bus drivers # # CONFIG_I2C_PCA_PLATFORM is not set # CONFIG_I2C_STUB is not set # # Miscellaneous I2C Chip support # # CONFIG_SENSORS_TSL2550 is not set # CONFIG_I2C_DEBUG_CORE is not set # CONFIG_I2C_DEBUG_ALGO is not set # CONFIG_I2C_DEBUG_BUS is not set # CONFIG_I2C_DEBUG_CHIP is not set CONFIG_SPI=y CONFIG_SPI_MASTER=y # # SPI Master Controller Drivers # CONFIG_SPI_DAVINCI=y CONFIG_SPI_BITBANG=y # CONFIG_SPI_GPIO is not set # CONFIG_SPI_XILINX is not set # CONFIG_SPI_DESIGNWARE is not set # # SPI Protocol Masters # # CONFIG_SPI_SPIDEV is not set # CONFIG_SPI_TLE62X0 is not set # # PPS support # # CONFIG_PPS is not set CONFIG_ARCH_REQUIRE_GPIOLIB=y CONFIG_GPIOLIB=y # CONFIG_GPIO_SYSFS is not set # # Memory mapped GPIO expanders: # # # I2C GPIO expanders: # # CONFIG_GPIO_MAX732X is not set CONFIG_GPIO_PCA953X=y CONFIG_GPIO_PCF857X=y # CONFIG_GPIO_ADP5588 is not set # # PCI GPIO expanders: # # # SPI GPIO expanders: # # CONFIG_GPIO_MAX7301 is not set # CONFIG_GPIO_MCP23S08 is not set # CONFIG_GPIO_MC33880 is not set # # AC97 GPIO expanders: # # CONFIG_W1 is not set # CONFIG_POWER_SUPPLY is not set # CONFIG_HWMON is not set # CONFIG_THERMAL is not set CONFIG_WATCHDOG=y # CONFIG_WATCHDOG_NOWAYOUT is not set # # Watchdog Device Drivers # # CONFIG_SOFT_WATCHDOG is not set CONFIG_DAVINCI_WATCHDOG=y # # USB-based Watchdog Cards # # CONFIG_USBPCWATCHDOG is not set CONFIG_SSB_POSSIBLE=y # # Sonics Silicon Backplane # # CONFIG_SSB is not set # # Multifunction device drivers # # CONFIG_MFD_CORE is not set # CONFIG_MFD_SM501 is not set # CONFIG_MFD_ASIC3 is not set # CONFIG_HTC_EGPIO is not set # CONFIG_HTC_PASIC3 is not set # CONFIG_TPS65010 is not set CONFIG_TPS6507x=y # CONFIG_TWL4030_CORE is not set # CONFIG_MFD_TMIO is not set # CONFIG_MFD_T7L66XB is not set # CONFIG_MFD_TC6387XB is not set # CONFIG_MFD_TC6393XB is not set # CONFIG_PMIC_DA903X is not set # CONFIG_PMIC_ADP5520 is not set # CONFIG_MFD_WM8400 is not set # CONFIG_MFD_WM831X is not set # CONFIG_MFD_WM8350_I2C is not set # CONFIG_MFD_PCF50633 is not set # CONFIG_MFD_MC13783 is not set # CONFIG_AB3100_CORE is not set # CONFIG_EZX_PCAP is not set # CONFIG_MFD_88PM8607 is not set # CONFIG_AB4500_CORE is not set CONFIG_REGULATOR=y # CONFIG_REGULATOR_DEBUG is not set # CONFIG_REGULATOR_FIXED_VOLTAGE is not set # CONFIG_REGULATOR_VIRTUAL_CONSUMER is not set # CONFIG_REGULATOR_USERSPACE_CONSUMER is not set # CONFIG_REGULATOR_BQ24022 is not set # CONFIG_REGULATOR_MAX1586 is not set # CONFIG_REGULATOR_MAX8660 is not set # CONFIG_REGULATOR_LP3971 is not set # CONFIG_REGULATOR_TPS65023 is not set CONFIG_REGULATOR_TPS6507X=y CONFIG_MEDIA_SUPPORT=y # # Multimedia core support # CONFIG_VIDEO_DEV=y CONFIG_VIDEO_V4L2_COMMON=y CONFIG_VIDEO_ALLOW_V4L1=y CONFIG_VIDEO_V4L1_COMPAT=y # CONFIG_DVB_CORE is not set CONFIG_VIDEO_MEDIA=y # # Multimedia drivers # CONFIG_IR_CORE=y CONFIG_VIDEO_IR=y # CONFIG_MEDIA_ATTACH is not set CONFIG_MEDIA_TUNER=y # CONFIG_MEDIA_TUNER_CUSTOMISE is not set CONFIG_MEDIA_TUNER_SIMPLE=y CONFIG_MEDIA_TUNER_TDA8290=y CONFIG_MEDIA_TUNER_TDA9887=y CONFIG_MEDIA_TUNER_TEA5761=y CONFIG_MEDIA_TUNER_TEA5767=y CONFIG_MEDIA_TUNER_MT20XX=y CONFIG_MEDIA_TUNER_XC2028=y CONFIG_MEDIA_TUNER_XC5000=y CONFIG_MEDIA_TUNER_MC44S803=y CONFIG_VIDEO_V4L2=y CONFIG_VIDEO_V4L1=y CONFIG_VIDEOBUF_GEN=y CONFIG_VIDEOBUF_DMA_CONTIG=y CONFIG_VIDEO_CAPTURE_DRIVERS=y # CONFIG_VIDEO_ADV_DEBUG is not set # CONFIG_VIDEO_FIXED_MINOR_RANGES is not set # CONFIG_VIDEO_HELPER_CHIPS_AUTO is not set # CONFIG_VIDEO_IR_I2C is not set # # Encoders/decoders and other helper chips # # # Audio decoders # # CONFIG_VIDEO_TVAUDIO is not set # CONFIG_VIDEO_TDA7432 is not set # CONFIG_VIDEO_TDA9840 is not set # CONFIG_VIDEO_TDA9875 is not set # CONFIG_VIDEO_TEA6415C is not set # CONFIG_VIDEO_TEA6420 is not set # CONFIG_VIDEO_MSP3400 is not set # CONFIG_VIDEO_CS5345 is not set # CONFIG_VIDEO_CS53L32A is not set # CONFIG_VIDEO_M52790 is not set # CONFIG_VIDEO_TLV320AIC23B is not set # CONFIG_VIDEO_WM8775 is not set # CONFIG_VIDEO_WM8739 is not set # CONFIG_VIDEO_VP27SMPX is not set # # RDS decoders # # CONFIG_VIDEO_SAA6588 is not set # # Video decoders # # CONFIG_VIDEO_ADV7180 is not set # CONFIG_VIDEO_BT819 is not set # CONFIG_VIDEO_BT856 is not set # CONFIG_VIDEO_BT866 is not set # CONFIG_VIDEO_KS0127 is not set # CONFIG_VIDEO_OV7670 is not set # CONFIG_VIDEO_MT9V011 is not set # CONFIG_VIDEO_TCM825X is not set # CONFIG_VIDEO_SAA7110 is not set # CONFIG_VIDEO_SAA711X is not set # CONFIG_VIDEO_SAA717X is not set # CONFIG_VIDEO_SAA7191 is not set CONFIG_VIDEO_TVP514X=y # CONFIG_VIDEO_TVP5150 is not set # CONFIG_VIDEO_VPX3220 is not set # # Video and audio decoders # # CONFIG_VIDEO_CX25840 is not set # # MPEG video encoders # # CONFIG_VIDEO_CX2341X is not set # # Video encoders # # CONFIG_VIDEO_SAA7127 is not set # CONFIG_VIDEO_SAA7185 is not set # CONFIG_VIDEO_ADV7170 is not set # CONFIG_VIDEO_ADV7175 is not set CONFIG_VIDEO_THS7303=y CONFIG_VIDEO_ADV7343=y # # Video improvement chips # # CONFIG_VIDEO_UPD64031A is not set # CONFIG_VIDEO_UPD64083 is not set CONFIG_VIDEO_DAVINCI_VPIF_DISPLAY=y CONFIG_VIDEO_DAVINCI_VPIF_CAPTURE=y CONFIG_VIDEO_DAVINCI_VPIF=y # CONFIG_VIDEO_VIVI is not set # CONFIG_VIDEO_VPSS_SYSTEM is not set # CONFIG_VIDEO_VPFE_CAPTURE is not set # CONFIG_VIDEO_CPIA is not set # CONFIG_VIDEO_CPIA2 is not set # CONFIG_VIDEO_SAA5246A is not set # CONFIG_VIDEO_SAA5249 is not set # CONFIG_SOC_CAMERA is not set CONFIG_V4L_USB_DRIVERS=y CONFIG_USB_VIDEO_CLASS=y # CONFIG_USB_VIDEO_CLASS_INPUT_EVDEV is not set # CONFIG_USB_GSPCA is not set # CONFIG_VIDEO_PVRUSB2 is not set # CONFIG_VIDEO_HDPVR is not set # CONFIG_VIDEO_EM28XX is not set # CONFIG_VIDEO_CX231XX is not set # CONFIG_VIDEO_USBVISION is not set # CONFIG_USB_VICAM is not set # CONFIG_USB_IBMCAM is not set # CONFIG_USB_KONICAWC is not set # CONFIG_USB_QUICKCAM_MESSENGER is not set # CONFIG_USB_ET61X251 is not set # CONFIG_VIDEO_OVCAMCHIP is not set # CONFIG_USB_OV511 is not set # CONFIG_USB_SE401 is not set # CONFIG_USB_SN9C102 is not set # CONFIG_USB_STV680 is not set # CONFIG_USB_ZC0301 is not set # CONFIG_USB_PWC is not set # CONFIG_USB_PWC_INPUT_EVDEV is not set # CONFIG_USB_ZR364XX is not set # CONFIG_USB_STKWEBCAM is not set # CONFIG_USB_S2255 is not set # CONFIG_RADIO_ADAPTERS is not set # CONFIG_DAB is not set # # Graphics support # # CONFIG_VGASTATE is not set # CONFIG_VIDEO_OUTPUT_CONTROL is not set CONFIG_FB=y # CONFIG_FIRMWARE_EDID is not set # CONFIG_FB_DDC is not set # CONFIG_FB_BOOT_VESA_SUPPORT is not set CONFIG_FB_CFB_FILLRECT=y CONFIG_FB_CFB_COPYAREA=y CONFIG_FB_CFB_IMAGEBLIT=y # CONFIG_FB_CFB_REV_PIXELS_IN_BYTE is not set # CONFIG_FB_SYS_FILLRECT is not set # CONFIG_FB_SYS_COPYAREA is not set # CONFIG_FB_SYS_IMAGEBLIT is not set # CONFIG_FB_FOREIGN_ENDIAN is not set # CONFIG_FB_SYS_FOPS is not set # CONFIG_FB_SVGALIB is not set # CONFIG_FB_MACMODES is not set # CONFIG_FB_BACKLIGHT is not set # CONFIG_FB_MODE_HELPERS is not set # CONFIG_FB_TILEBLITTING is not set # # Frame buffer hardware drivers # # CONFIG_FB_S1D13XXX is not set # CONFIG_FB_DAVINCI is not set # CONFIG_FB_VIRTUAL is not set CONFIG_FB_DA8XX=y # CONFIG_FB_METRONOME is not set # CONFIG_FB_MB862XX is not set # CONFIG_FB_BROADSHEET is not set # CONFIG_BACKLIGHT_LCD_SUPPORT is not set # # Display device support # # CONFIG_DISPLAY_SUPPORT is not set # # Console display driver support # # CONFIG_VGA_CONSOLE is not set CONFIG_DUMMY_CONSOLE=y CONFIG_FRAMEBUFFER_CONSOLE=y # CONFIG_FRAMEBUFFER_CONSOLE_DETECT_PRIMARY is not set # CONFIG_FRAMEBUFFER_CONSOLE_ROTATION is not set # CONFIG_FONTS is not set CONFIG_FONT_8x8=y CONFIG_FONT_8x16=y CONFIG_LOGO=y CONFIG_LOGO_LINUX_MONO=y CONFIG_LOGO_LINUX_VGA16=y CONFIG_LOGO_LINUX_CLUT224=y CONFIG_SOUND=y # CONFIG_SOUND_OSS_CORE is not set CONFIG_SND=y CONFIG_SND_TIMER=y CONFIG_SND_PCM=y CONFIG_SND_HWDEP=y CONFIG_SND_RAWMIDI=y CONFIG_SND_JACK=y # CONFIG_SND_SEQUENCER is not set # CONFIG_SND_MIXER_OSS is not set # CONFIG_SND_PCM_OSS is not set # CONFIG_SND_HRTIMER is not set # CONFIG_SND_DYNAMIC_MINORS is not set CONFIG_SND_SUPPORT_OLD_API=y CONFIG_SND_VERBOSE_PROCFS=y # CONFIG_SND_VERBOSE_PRINTK is not set # CONFIG_SND_DEBUG is not set # CONFIG_SND_RAWMIDI_SEQ is not set # CONFIG_SND_OPL3_LIB_SEQ is not set # CONFIG_SND_OPL4_LIB_SEQ is not set # CONFIG_SND_SBAWE_SEQ is not set # CONFIG_SND_EMU10K1_SEQ is not set CONFIG_SND_DRIVERS=y # CONFIG_SND_DUMMY is not set # CONFIG_SND_MTPAV is not set # CONFIG_SND_SERIAL_U16550 is not set # CONFIG_SND_MPU401 is not set CONFIG_SND_ARM=y CONFIG_SND_SPI=y CONFIG_SND_USB=y CONFIG_SND_USB_AUDIO=y # CONFIG_SND_USB_CAIAQ is not set CONFIG_SND_SOC=y CONFIG_SND_DAVINCI_SOC=y CONFIG_SND_DAVINCI_SOC_MCASP=y CONFIG_SND_DA850_SOC_EVM=y CONFIG_SND_SOC_I2C_AND_SPI=y # CONFIG_SND_SOC_ALL_CODECS is not set CONFIG_SND_SOC_TLV320AIC3X=y # CONFIG_SOUND_PRIME is not set CONFIG_HID_SUPPORT=y CONFIG_HID=y # CONFIG_HIDRAW is not set # # USB Input Devices # CONFIG_USB_HID=y # CONFIG_HID_PID is not set # CONFIG_USB_HIDDEV is not set # # Special HID drivers # # CONFIG_HID_A4TECH is not set # CONFIG_HID_APPLE is not set # CONFIG_HID_BELKIN is not set # CONFIG_HID_CHERRY is not set # CONFIG_HID_CHICONY is not set # CONFIG_HID_CYPRESS is not set # CONFIG_HID_DRAGONRISE is not set # CONFIG_HID_EZKEY is not set # CONFIG_HID_KYE is not set # CONFIG_HID_GYRATION is not set # CONFIG_HID_TWINHAN is not set # CONFIG_HID_KENSINGTON is not set # CONFIG_HID_LOGITECH is not set # CONFIG_HID_MICROSOFT is not set # CONFIG_HID_MONTEREY is not set # CONFIG_HID_NTRIG is not set # CONFIG_HID_PANTHERLORD is not set # CONFIG_HID_PETALYNX is not set # CONFIG_HID_SAMSUNG is not set # CONFIG_HID_SONY is not set # CONFIG_HID_SUNPLUS is not set # CONFIG_HID_GREENASIA is not set # CONFIG_HID_SMARTJOYPLUS is not set # CONFIG_HID_TOPSEED is not set # CONFIG_HID_THRUSTMASTER is not set # CONFIG_HID_ZEROPLUS is not set CONFIG_USB_SUPPORT=y CONFIG_USB_ARCH_HAS_HCD=y CONFIG_USB_ARCH_HAS_OHCI=y # CONFIG_USB_ARCH_HAS_EHCI is not set CONFIG_USB=y # CONFIG_USB_DEBUG is not set # CONFIG_USB_ANNOUNCE_NEW_DEVICES is not set # # Miscellaneous USB options # # CONFIG_USB_DEVICEFS is not set # CONFIG_USB_DEVICE_CLASS is not set # CONFIG_USB_DYNAMIC_MINORS is not set CONFIG_USB_SUSPEND=y # CONFIG_USB_OTG is not set # CONFIG_USB_OTG_WHITELIST is not set # CONFIG_USB_OTG_BLACKLIST_HUB is not set # CONFIG_USB_MON is not set # CONFIG_USB_WUSB is not set # CONFIG_USB_WUSB_CBAF is not set # # USB Host Controller Drivers # # CONFIG_USB_C67X00_HCD is not set # CONFIG_USB_OXU210HP_HCD is not set # CONFIG_USB_ISP116X_HCD is not set # CONFIG_USB_ISP1760_HCD is not set # CONFIG_USB_ISP1362_HCD is not set CONFIG_USB_OHCI_HCD=y # CONFIG_USB_OHCI_BIG_ENDIAN_DESC is not set # CONFIG_USB_OHCI_BIG_ENDIAN_MMIO is not set CONFIG_USB_OHCI_LITTLE_ENDIAN=y # CONFIG_USB_SL811_HCD is not set # CONFIG_USB_R8A66597_HCD is not set # CONFIG_USB_HWA_HCD is not set CONFIG_USB_MUSB_HDRC=y CONFIG_USB_MUSB_SOC=y CONFIG_USB_MUSB_HOST=y # CONFIG_USB_MUSB_PERIPHERAL is not set # CONFIG_USB_MUSB_DUAL_ROLE is not set # CONFIG_USB_MUSB_OTG is not set CONFIG_USB_MUSB_HDRC_HCD=y # CONFIG_MUSB_PIO_ONLY is not set # CONFIG_USB_INVENTRA_DMA is not set # CONFIG_USB_TI_CPPI_DMA is not set CONFIG_USB_TI_CPPI41_DMA=y CONFIG_USB_MUSB_DEBUG=y # # USB Device Class drivers # # CONFIG_USB_ACM is not set # CONFIG_USB_PRINTER is not set # CONFIG_USB_WDM is not set # CONFIG_USB_TMC is not set # # NOTE: USB_STORAGE depends on SCSI but BLK_DEV_SD may # # # also be needed; see USB_STORAGE Help for more info # CONFIG_USB_STORAGE=y # CONFIG_USB_STORAGE_DEBUG is not set # CONFIG_USB_STORAGE_DATAFAB is not set # CONFIG_USB_STORAGE_FREECOM is not set # CONFIG_USB_STORAGE_ISD200 is not set # CONFIG_USB_STORAGE_USBAT is not set # CONFIG_USB_STORAGE_SDDR09 is not set # CONFIG_USB_STORAGE_SDDR55 is not set # CONFIG_USB_STORAGE_JUMPSHOT is not set # CONFIG_USB_STORAGE_ALAUDA is not set # CONFIG_USB_STORAGE_ONETOUCH is not set # CONFIG_USB_STORAGE_KARMA is not set # CONFIG_USB_STORAGE_CYPRESS_ATACB is not set # CONFIG_USB_LIBUSUAL is not set # # USB Imaging devices # # CONFIG_USB_MDC800 is not set # CONFIG_USB_MICROTEK is not set # # USB port drivers # # CONFIG_USB_SERIAL is not set # # USB Miscellaneous drivers # # CONFIG_USB_EMI62 is not set # CONFIG_USB_EMI26 is not set # CONFIG_USB_ADUTUX is not set # CONFIG_USB_SEVSEG is not set # CONFIG_USB_RIO500 is not set # CONFIG_USB_LEGOTOWER is not set # CONFIG_USB_LCD is not set # CONFIG_USB_BERRY_CHARGE is not set # CONFIG_USB_LED is not set # CONFIG_USB_CYPRESS_CY7C63 is not set # CONFIG_USB_CYTHERM is not set # CONFIG_USB_IDMOUSE is not set # CONFIG_USB_FTDI_ELAN is not set # CONFIG_USB_APPLEDISPLAY is not set # CONFIG_USB_SISUSBVGA is not set # CONFIG_USB_LD is not set # CONFIG_USB_TRANCEVIBRATOR is not set # CONFIG_USB_IOWARRIOR is not set # CONFIG_USB_TEST is not set # CONFIG_USB_ISIGHTFW is not set # CONFIG_USB_VST is not set # CONFIG_USB_GADGET is not set # # OTG and related infrastructure # CONFIG_USB_OTG_UTILS=y # CONFIG_USB_GPIO_VBUS is not set # CONFIG_USB_ULPI is not set CONFIG_NOP_USB_XCEIV=y CONFIG_MMC=y # CONFIG_MMC_DEBUG is not set # CONFIG_MMC_UNSAFE_RESUME is not set # # MMC/SD/SDIO Card Drivers # CONFIG_MMC_BLOCK=y CONFIG_MMC_BLOCK_BOUNCE=y # CONFIG_SDIO_UART is not set # CONFIG_MMC_TEST is not set # # MMC/SD/SDIO Host Controller Drivers # # CONFIG_MMC_SDHCI is not set # CONFIG_MMC_AT91 is not set # CONFIG_MMC_ATMELMCI is not set CONFIG_MMC_DAVINCI=y # CONFIG_MMC_SPI is not set # CONFIG_MEMSTICK is not set # CONFIG_NEW_LEDS is not set # CONFIG_ACCESSIBILITY is not set CONFIG_RTC_LIB=y CONFIG_RTC_CLASS=y CONFIG_RTC_HCTOSYS=y CONFIG_RTC_HCTOSYS_DEVICE="rtc0" # CONFIG_RTC_DEBUG is not set # # RTC interfaces # CONFIG_RTC_INTF_SYSFS=y CONFIG_RTC_INTF_PROC=y CONFIG_RTC_INTF_DEV=y # CONFIG_RTC_INTF_DEV_UIE_EMUL is not set # CONFIG_RTC_DRV_TEST is not set # # I2C RTC drivers # # CONFIG_RTC_DRV_DS1307 is not set # CONFIG_RTC_DRV_DS1374 is not set # CONFIG_RTC_DRV_DS1672 is not set # CONFIG_RTC_DRV_MAX6900 is not set # CONFIG_RTC_DRV_RS5C372 is not set # CONFIG_RTC_DRV_ISL1208 is not set # CONFIG_RTC_DRV_X1205 is not set # CONFIG_RTC_DRV_PCF8563 is not set # CONFIG_RTC_DRV_PCF8583 is not set # CONFIG_RTC_DRV_M41T80 is not set # CONFIG_RTC_DRV_BQ32K is not set # CONFIG_RTC_DRV_S35390A is not set # CONFIG_RTC_DRV_FM3130 is not set # CONFIG_RTC_DRV_RX8581 is not set # CONFIG_RTC_DRV_RX8025 is not set # # SPI RTC drivers # # CONFIG_RTC_DRV_M41T94 is not set # CONFIG_RTC_DRV_DS1305 is not set # CONFIG_RTC_DRV_DS1390 is not set # CONFIG_RTC_DRV_MAX6902 is not set # CONFIG_RTC_DRV_R9701 is not set # CONFIG_RTC_DRV_RS5C348 is not set # CONFIG_RTC_DRV_DS3234 is not set # CONFIG_RTC_DRV_PCF2123 is not set # # Platform RTC drivers # # CONFIG_RTC_DRV_CMOS is not set # CONFIG_RTC_DRV_DS1286 is not set # CONFIG_RTC_DRV_DS1511 is not set # CONFIG_RTC_DRV_DS1553 is not set # CONFIG_RTC_DRV_DS1742 is not set # CONFIG_RTC_DRV_STK17TA8 is not set # CONFIG_RTC_DRV_M48T86 is not set # CONFIG_RTC_DRV_M48T35 is not set # CONFIG_RTC_DRV_M48T59 is not set # CONFIG_RTC_DRV_MSM6242 is not set # CONFIG_RTC_DRV_BQ4802 is not set # CONFIG_RTC_DRV_RP5C01 is not set # CONFIG_RTC_DRV_V3020 is not set # # on-CPU RTC drivers # CONFIG_RTC_DRV_OMAP=y # CONFIG_DMADEVICES is not set # CONFIG_AUXDISPLAY is not set # CONFIG_UIO is not set # # TI VLYNQ # # CONFIG_STAGING is not set # # File systems # CONFIG_EXT2_FS=y # CONFIG_EXT2_FS_XATTR is not set # CONFIG_EXT2_FS_XIP is not set CONFIG_EXT3_FS=y # CONFIG_EXT3_DEFAULTS_TO_ORDERED is not set CONFIG_EXT3_FS_XATTR=y # CONFIG_EXT3_FS_POSIX_ACL is not set # CONFIG_EXT3_FS_SECURITY is not set # CONFIG_EXT4_FS is not set CONFIG_JBD=y # CONFIG_JBD_DEBUG is not set CONFIG_FS_MBCACHE=y # CONFIG_REISERFS_FS is not set # CONFIG_JFS_FS is not set # CONFIG_FS_POSIX_ACL is not set # CONFIG_XFS_FS is not set # CONFIG_GFS2_FS is not set # CONFIG_OCFS2_FS is not set # CONFIG_BTRFS_FS is not set # CONFIG_NILFS2_FS is not set CONFIG_FILE_LOCKING=y CONFIG_FSNOTIFY=y CONFIG_DNOTIFY=y CONFIG_INOTIFY=y CONFIG_INOTIFY_USER=y # CONFIG_QUOTA is not set # CONFIG_AUTOFS_FS is not set CONFIG_AUTOFS4_FS=m # CONFIG_FUSE_FS is not set # # Caches # # CONFIG_FSCACHE is not set # # CD-ROM/DVD Filesystems # # CONFIG_ISO9660_FS is not set # CONFIG_UDF_FS is not set # # DOS/FAT/NT Filesystems # CONFIG_FAT_FS=y CONFIG_MSDOS_FS=y CONFIG_VFAT_FS=y CONFIG_FAT_DEFAULT_CODEPAGE=437 CONFIG_FAT_DEFAULT_IOCHARSET="iso8859-1" # CONFIG_NTFS_FS is not set # # Pseudo filesystems # CONFIG_PROC_FS=y CONFIG_PROC_SYSCTL=y CONFIG_PROC_PAGE_MONITOR=y CONFIG_SYSFS=y CONFIG_TMPFS=y # CONFIG_TMPFS_POSIX_ACL is not set # CONFIG_HUGETLB_PAGE is not set # CONFIG_CONFIGFS_FS is not set CONFIG_MISC_FILESYSTEMS=y # CONFIG_ADFS_FS is not set # CONFIG_AFFS_FS is not set # CONFIG_HFS_FS is not set # CONFIG_HFSPLUS_FS is not set # CONFIG_BEFS_FS is not set # CONFIG_BFS_FS is not set # CONFIG_EFS_FS is not set CONFIG_JFFS2_FS=y CONFIG_JFFS2_FS_DEBUG=0 CONFIG_JFFS2_FS_WRITEBUFFER=y # CONFIG_JFFS2_FS_WBUF_VERIFY is not set # CONFIG_JFFS2_SUMMARY is not set # CONFIG_JFFS2_FS_XATTR is not set # CONFIG_JFFS2_COMPRESSION_OPTIONS is not set CONFIG_JFFS2_ZLIB=y # CONFIG_JFFS2_LZO is not set CONFIG_JFFS2_RTIME=y # CONFIG_JFFS2_RUBIN is not set CONFIG_CRAMFS=y # CONFIG_SQUASHFS is not set # CONFIG_VXFS_FS is not set CONFIG_MINIX_FS=m # CONFIG_OMFS_FS is not set # CONFIG_HPFS_FS is not set # CONFIG_QNX4FS_FS is not set # CONFIG_ROMFS_FS is not set # CONFIG_SYSV_FS is not set # CONFIG_UFS_FS is not set CONFIG_NETWORK_FILESYSTEMS=y CONFIG_NFS_FS=y CONFIG_NFS_V3=y # CONFIG_NFS_V3_ACL is not set # CONFIG_NFS_V4 is not set CONFIG_ROOT_NFS=y CONFIG_NFSD=m CONFIG_NFSD_V3=y # CONFIG_NFSD_V3_ACL is not set # CONFIG_NFSD_V4 is not set CONFIG_LOCKD=y CONFIG_LOCKD_V4=y CONFIG_EXPORTFS=m CONFIG_NFS_COMMON=y CONFIG_SUNRPC=y # CONFIG_RPCSEC_GSS_KRB5 is not set # CONFIG_RPCSEC_GSS_SPKM3 is not set CONFIG_SMB_FS=m # CONFIG_SMB_NLS_DEFAULT is not set # CONFIG_CIFS is not set # CONFIG_NCP_FS is not set # CONFIG_CODA_FS is not set # CONFIG_AFS_FS is not set # # Partition Types # CONFIG_PARTITION_ADVANCED=y # CONFIG_ACORN_PARTITION is not set # CONFIG_OSF_PARTITION is not set # CONFIG_AMIGA_PARTITION is not set # CONFIG_ATARI_PARTITION is not set # CONFIG_MAC_PARTITION is not set CONFIG_MSDOS_PARTITION=y # CONFIG_BSD_DISKLABEL is not set # CONFIG_MINIX_SUBPARTITION is not set # CONFIG_SOLARIS_X86_PARTITION is not set # CONFIG_UNIXWARE_DISKLABEL is not set # CONFIG_LDM_PARTITION is not set # CONFIG_SGI_PARTITION is not set # CONFIG_ULTRIX_PARTITION is not set # CONFIG_SUN_PARTITION is not set # CONFIG_KARMA_PARTITION is not set # CONFIG_EFI_PARTITION is not set # CONFIG_SYSV68_PARTITION is not set CONFIG_NLS=y CONFIG_NLS_DEFAULT="iso8859-1" CONFIG_NLS_CODEPAGE_437=y # CONFIG_NLS_CODEPAGE_737 is not set # CONFIG_NLS_CODEPAGE_775 is not set # CONFIG_NLS_CODEPAGE_850 is not set # CONFIG_NLS_CODEPAGE_852 is not set # CONFIG_NLS_CODEPAGE_855 is not set # CONFIG_NLS_CODEPAGE_857 is not set # CONFIG_NLS_CODEPAGE_860 is not set # CONFIG_NLS_CODEPAGE_861 is not set # CONFIG_NLS_CODEPAGE_862 is not set # CONFIG_NLS_CODEPAGE_863 is not set # CONFIG_NLS_CODEPAGE_864 is not set # CONFIG_NLS_CODEPAGE_865 is not set # CONFIG_NLS_CODEPAGE_866 is not set # CONFIG_NLS_CODEPAGE_869 is not set # CONFIG_NLS_CODEPAGE_936 is not set # CONFIG_NLS_CODEPAGE_950 is not set # CONFIG_NLS_CODEPAGE_932 is not set # CONFIG_NLS_CODEPAGE_949 is not set # CONFIG_NLS_CODEPAGE_874 is not set # CONFIG_NLS_ISO8859_8 is not set # CONFIG_NLS_CODEPAGE_1250 is not set # CONFIG_NLS_CODEPAGE_1251 is not set CONFIG_NLS_ASCII=m CONFIG_NLS_ISO8859_1=y # CONFIG_NLS_ISO8859_2 is not set # CONFIG_NLS_ISO8859_3 is not set # CONFIG_NLS_ISO8859_4 is not set # CONFIG_NLS_ISO8859_5 is not set # CONFIG_NLS_ISO8859_6 is not set # CONFIG_NLS_ISO8859_7 is not set # CONFIG_NLS_ISO8859_9 is not set # CONFIG_NLS_ISO8859_13 is not set # CONFIG_NLS_ISO8859_14 is not set # CONFIG_NLS_ISO8859_15 is not set # CONFIG_NLS_KOI8_R is not set # CONFIG_NLS_KOI8_U is not set CONFIG_NLS_UTF8=m # CONFIG_DLM is not set # # Kernel hacking # # CONFIG_PRINTK_TIME is not set # CONFIG_ENABLE_WARN_DEPRECATED is not set # CONFIG_ENABLE_MUST_CHECK is not set CONFIG_FRAME_WARN=1024 # CONFIG_MAGIC_SYSRQ is not set # CONFIG_STRIP_ASM_SYMS is not set # CONFIG_UNUSED_SYMBOLS is not set CONFIG_DEBUG_FS=y # CONFIG_HEADERS_CHECK is not set # CONFIG_DEBUG_KERNEL is not set # CONFIG_SLUB_DEBUG_ON is not set # CONFIG_SLUB_STATS is not set CONFIG_DEBUG_BUGVERBOSE=y # CONFIG_DEBUG_MEMORY_INIT is not set CONFIG_FRAME_POINTER=y # CONFIG_RCU_CPU_STALL_DETECTOR is not set # CONFIG_LATENCYTOP is not set # CONFIG_SYSCTL_SYSCALL_CHECK is not set CONFIG_HAVE_FUNCTION_TRACER=y CONFIG_TRACING_SUPPORT=y # CONFIG_FTRACE is not set # CONFIG_DYNAMIC_DEBUG is not set # CONFIG_SAMPLES is not set CONFIG_HAVE_ARCH_KGDB=y # CONFIG_ARM_UNWIND is not set # CONFIG_DEBUG_USER is not set # CONFIG_OC_ETM is not set # # Security options # # CONFIG_KEYS is not set # CONFIG_SECURITY is not set # CONFIG_SECURITYFS is not set # CONFIG_DEFAULT_SECURITY_SELINUX is not set # CONFIG_DEFAULT_SECURITY_SMACK is not set # CONFIG_DEFAULT_SECURITY_TOMOYO is not set CONFIG_DEFAULT_SECURITY_DAC=y CONFIG_DEFAULT_SECURITY="" CONFIG_CRYPTO=y # # Crypto core or helper # # CONFIG_CRYPTO_MANAGER is not set # CONFIG_CRYPTO_MANAGER2 is not set # CONFIG_CRYPTO_GF128MUL is not set # CONFIG_CRYPTO_NULL is not set # CONFIG_CRYPTO_CRYPTD is not set # CONFIG_CRYPTO_AUTHENC is not set # CONFIG_CRYPTO_TEST is not set # # Authenticated Encryption with Associated Data # # CONFIG_CRYPTO_CCM is not set # CONFIG_CRYPTO_GCM is not set # CONFIG_CRYPTO_SEQIV is not set # # Block modes # # CONFIG_CRYPTO_CBC is not set # CONFIG_CRYPTO_CTR is not set # CONFIG_CRYPTO_CTS is not set # CONFIG_CRYPTO_ECB is not set # CONFIG_CRYPTO_LRW is not set # CONFIG_CRYPTO_PCBC is not set # CONFIG_CRYPTO_XTS is not set # # Hash modes # # CONFIG_CRYPTO_HMAC is not set # CONFIG_CRYPTO_XCBC is not set # CONFIG_CRYPTO_VMAC is not set # # Digest # # CONFIG_CRYPTO_CRC32C is not set # CONFIG_CRYPTO_GHASH is not set # CONFIG_CRYPTO_MD4 is not set # CONFIG_CRYPTO_MD5 is not set # CONFIG_CRYPTO_MICHAEL_MIC is not set # CONFIG_CRYPTO_RMD128 is not set # CONFIG_CRYPTO_RMD160 is not set # CONFIG_CRYPTO_RMD256 is not set # CONFIG_CRYPTO_RMD320 is not set # CONFIG_CRYPTO_SHA1 is not set # CONFIG_CRYPTO_SHA256 is not set # CONFIG_CRYPTO_SHA512 is not set # CONFIG_CRYPTO_TGR192 is not set # CONFIG_CRYPTO_WP512 is not set # # Ciphers # # CONFIG_CRYPTO_AES is not set # CONFIG_CRYPTO_ANUBIS is not set # CONFIG_CRYPTO_ARC4 is not set # CONFIG_CRYPTO_BLOWFISH is not set # CONFIG_CRYPTO_CAMELLIA is not set # CONFIG_CRYPTO_CAST5 is not set # CONFIG_CRYPTO_CAST6 is not set # CONFIG_CRYPTO_DES is not set # CONFIG_CRYPTO_FCRYPT is not set # CONFIG_CRYPTO_KHAZAD is not set # CONFIG_CRYPTO_SALSA20 is not set # CONFIG_CRYPTO_SEED is not set # CONFIG_CRYPTO_SERPENT is not set # CONFIG_CRYPTO_TEA is not set # CONFIG_CRYPTO_TWOFISH is not set # # Compression # # CONFIG_CRYPTO_DEFLATE is not set # CONFIG_CRYPTO_ZLIB is not set # CONFIG_CRYPTO_LZO is not set # # Random Number Generation # # CONFIG_CRYPTO_ANSI_CPRNG is not set # CONFIG_CRYPTO_HW is not set # CONFIG_BINARY_PRINTF is not set # # Library routines # CONFIG_BITREVERSE=y CONFIG_GENERIC_FIND_LAST_BIT=y CONFIG_CRC_CCITT=m # CONFIG_CRC16 is not set CONFIG_CRC_T10DIF=m # CONFIG_CRC_ITU_T is not set CONFIG_CRC32=y # CONFIG_CRC7 is not set # CONFIG_LIBCRC32C is not set CONFIG_ZLIB_INFLATE=y CONFIG_ZLIB_DEFLATE=y CONFIG_DECOMPRESS_GZIP=y CONFIG_GENERIC_ALLOCATOR=y CONFIG_HAS_IOMEM=y CONFIG_HAS_IOPORT=y CONFIG_HAS_DMA=y CONFIG_NLATTR=y
and all the commands used to build the kernel:
pfreire@pfreire-Latitude-E6410:~/SDKs/DaVinci-PSP-SDK-03.20.00.14/src/kernel/linux-03.20.00.14$ make distclean ARCH=arm CROSS_COMPILE=arm-none-eabi- CLEAN arch/arm/boot/compressed CLEAN arch/arm/boot CLEAN /home/pfreire/SDKs/DaVinci-PSP-SDK-03.20.00.14/src/kernel/linux-03.20.00.14 CLEAN arch/arm/kernel CLEAN drivers/char CLEAN drivers/video/logo CLEAN kernel CLEAN lib CLEAN usr CLEAN .tmp_versions CLEAN vmlinux System.map .tmp_kallsyms2.S .tmp_kallsyms1.o .tmp_kallsyms2.o .tmp_kallsyms1.S .tmp_vmlinux1 .tmp_vmlinux2 .tmp_System.map CLEAN scripts/basic CLEAN scripts/genksyms CLEAN scripts/kconfig CLEAN scripts/mod CLEAN scripts CLEAN include/config include/generated CLEAN .config .config.old .version include/linux/version.h Module.symvers pfreire@pfreire-Latitude-E6410:~/SDKs/DaVinci-PSP-SDK-03.20.00.14/src/kernel/linux-03.20.00.14$ make da850_omapl138_defconfig ARCH=arm CROSS_COMPILE=arm-none-ea bi- HOSTCC scripts/basic/fixdep HOSTCC scripts/basic/docproc HOSTCC scripts/basic/hash HOSTCC scripts/kconfig/conf.o scripts/kconfig/conf.c: In function 'conf_sym': scripts/kconfig/conf.c:159:6: warning: variable 'type' set but not used [-Wunused-but-set-variable] int type; ^ scripts/kconfig/conf.c: In function 'conf_choice': scripts/kconfig/conf.c:231:6: warning: variable 'type' set but not used [-Wunused-but-set-variable] int type; ^ scripts/kconfig/conf.c:307:4: warning: ignoring return value of 'fgets', declared with attribute warn_unused_result [-Wunused-result] fgets(line, 128, stdin); ^ scripts/kconfig/conf.c: In function 'conf_askvalue': scripts/kconfig/conf.c:105:3: warning: ignoring return value of 'fgets', declared with attribute warn_unused_result [-Wunused-result] fgets(line, 128, stdin); ^ HOSTCC scripts/kconfig/kxgettext.o SHIPPED scripts/kconfig/zconf.tab.c SHIPPED scripts/kconfig/lex.zconf.c SHIPPED scripts/kconfig/zconf.hash.c HOSTCC scripts/kconfig/zconf.tab.o HOSTLD scripts/kconfig/conf # # configuration written to .config # pfreire@pfreire-Latitude-E6410:~/SDKs/DaVinci-PSP-SDK-03.20.00.14/src/kernel/linux-03.20.00.14$ make ARCH=arm CROSS_COMPILE=arm-none-eabi- menuconfig HOSTCC scripts/kconfig/lxdialog/checklist.o HOSTCC scripts/kconfig/lxdialog/inputbox.o HOSTCC scripts/kconfig/lxdialog/menubox.o HOSTCC scripts/kconfig/lxdialog/textbox.o scripts/kconfig/lxdialog/textbox.c: In function 'print_line': scripts/kconfig/lxdialog/textbox.c:323:9: warning: variable 'x' set but not used [-Wunused-but-set-variable] int y, x; ^ scripts/kconfig/lxdialog/textbox.c:323:6: warning: variable 'y' set but not used [-Wunused-but-set-variable] int y, x; ^ HOSTCC scripts/kconfig/lxdialog/util.o HOSTCC scripts/kconfig/lxdialog/yesno.o HOSTCC scripts/kconfig/mconf.o HOSTLD scripts/kconfig/mconf scripts/kconfig/mconf arch/arm/Kconfig # # configuration written to .config # *** End of Linux kernel configuration. *** Execute 'make' to build the kernel or try 'make help'. pfreire@pfreire-Latitude-E6410:~/SDKs/DaVinci-PSP-SDK-03.20.00.14/src/kernel/linux-03.20.00.14$ make uImage ARCH=arm CROSS_COMPILE=arm-none-eabi- scripts/kconfig/conf -s arch/arm/Kconfig CHK include/linux/version.h UPD include/linux/version.h CHK include/generated/utsrelease.h UPD include/generated/utsrelease.h Generating include/generated/mach-types.h CC kernel/bounds.s GEN include/generated/bounds.h CC arch/arm/kernel/asm-offsets.s GEN include/generated/asm-offsets.h CALL scripts/checksyscalls.sh HOSTCC scripts/genksyms/genksyms.o SHIPPED scripts/genksyms/lex.c SHIPPED scripts/genksyms/parse.h SHIPPED scripts/genksyms/keywords.c HOSTCC scripts/genksyms/lex.o SHIPPED scripts/genksyms/parse.c HOSTCC scripts/genksyms/parse.o HOSTLD scripts/genksyms/genksyms CC scripts/mod/empty.o HOSTCC scripts/mod/mk_elfconfig MKELF scripts/mod/elfconfig.h HOSTCC scripts/mod/file2alias.o HOSTCC scripts/mod/modpost.o HOSTCC scripts/mod/sumversion.o HOSTLD scripts/mod/modpost HOSTCC scripts/kallsyms scripts/kallsyms.c: In function 'read_symbol': scripts/kallsyms.c:112:4: warning: ignoring return value of 'fgets', declared with attribute warn_unused_result [-Wunused-result] fgets(str, 500, in); ^ HOSTCC scripts/pnmtologo HOSTCC scripts/conmakehash HOSTCC scripts/bin2c CC init/main.o In file included from include/linux/mempolicy.h:62:0, from init/main.c:52: include/linux/pagemap.h: In function 'fault_in_pages_readable': include/linux/pagemap.h:413:16: warning: variable 'c' set but not used [-Wunused-but-set-variable] volatile char c; ^ CHK include/generated/compile.h UPD include/generated/compile.h CC init/version.o CC init/do_mounts.o In file included from include/linux/nfs_fs.h:44:0, from init/do_mounts.c:19: include/linux/pagemap.h: In function 'fault_in_pages_readable': include/linux/pagemap.h:413:16: warning: variable 'c' set but not used [-Wunused-but-set-variable] volatile char c; ^ CC init/do_mounts_rd.o In file included from include/linux/blkdev.h:12:0, from init/do_mounts.h:2, from init/do_mounts_rd.c:11: include/linux/pagemap.h: In function 'fault_in_pages_readable': include/linux/pagemap.h:413:16: warning: variable 'c' set but not used [-Wunused-but-set-variable] volatile char c; ^ CC init/do_mounts_initrd.o In file included from include/linux/blkdev.h:12:0, from init/do_mounts.h:2, from init/do_mounts_initrd.c:11: include/linux/pagemap.h: In function 'fault_in_pages_readable': include/linux/pagemap.h:413:16: warning: variable 'c' set but not used [-Wunused-but-set-variable] volatile char c; ^ LD init/mounts.o CC init/initramfs.o CC init/calibrate.o LD init/built-in.o HOSTCC usr/gen_init_cpio GEN usr/initramfs_data.cpio AS usr/initramfs_data.o LD usr/built-in.o CC arch/arm/kernel/compat.o CC arch/arm/kernel/elf.o AS arch/arm/kernel/entry-armv.o AS arch/arm/kernel/entry-common.o CC arch/arm/kernel/irq.o CC arch/arm/kernel/process.o CC arch/arm/kernel/ptrace.o CC arch/arm/kernel/return_address.o CC arch/arm/kernel/setup.o CC arch/arm/kernel/signal.o arch/arm/kernel/signal.c: In function 'restore_sigframe': arch/arm/kernel/signal.c:193:30: warning: variable 'aux' set but not used [-Wunused-but-set-variable] struct aux_sigframe __user *aux; ^ CC arch/arm/kernel/sys_arm.o CC arch/arm/kernel/stacktrace.o CC arch/arm/kernel/time.o CC arch/arm/kernel/traps.o CC arch/arm/kernel/armksyms.o CC arch/arm/kernel/module.o CC arch/arm/kernel/io.o LD arch/arm/kernel/built-in.o AS arch/arm/kernel/head.o CC arch/arm/kernel/init_task.o LDS arch/arm/kernel/vmlinux.lds CC arch/arm/mm/dma-mapping.o CC arch/arm/mm/extable.o CC arch/arm/mm/fault.o CC arch/arm/mm/init.o CC arch/arm/mm/iomap.o CC arch/arm/mm/fault-armv.o In file included from arch/arm/mm/fault-armv.c:18:0: include/linux/pagemap.h: In function 'fault_in_pages_readable': include/linux/pagemap.h:413:16: warning: variable 'c' set but not used [-Wunused-but-set-variable] volatile char c; ^ CC arch/arm/mm/flush.o In file included from arch/arm/mm/flush.c:12:0: include/linux/pagemap.h: In function 'fault_in_pages_readable': include/linux/pagemap.h:413:16: warning: variable 'c' set but not used [-Wunused-but-set-variable] volatile char c; ^ CC arch/arm/mm/ioremap.o CC arch/arm/mm/mmap.o CC arch/arm/mm/pgd.o CC arch/arm/mm/mmu.o CC arch/arm/mm/vmregion.o CC arch/arm/mm/proc-syms.o CC arch/arm/mm/alignment.o arch/arm/mm/alignment.c: In function 'do_alignment': arch/arm/mm/alignment.c:294:15: warning: 'offset.un' may be used uninitialized in this function [-Wmaybe-uninitialized] offset.un = -offset.un; ^ arch/arm/mm/alignment.c:716:21: note: 'offset.un' was declared here union offset_union offset; ^ AS arch/arm/mm/abort-ev5tj.o AS arch/arm/mm/pabort-legacy.o CC arch/arm/mm/copypage-v4wb.o AS arch/arm/mm/tlb-v4wbi.o AS arch/arm/mm/proc-arm926.o LD arch/arm/mm/built-in.o CC arch/arm/common/clkdev.o LD arch/arm/common/built-in.o CC arch/arm/mach-davinci/time.o CC arch/arm/mach-davinci/clock.o CC arch/arm/mach-davinci/serial.o CC arch/arm/mach-davinci/io.o CC arch/arm/mach-davinci/psc.o CC arch/arm/mach-davinci/gpio.o CC arch/arm/mach-davinci/dma.o CC arch/arm/mach-davinci/usb.o CC arch/arm/mach-davinci/common.o CC arch/arm/mach-davinci/sram.o CC arch/arm/mach-davinci/aemif.o CC arch/arm/mach-davinci/mux.o CC arch/arm/mach-davinci/da850.o CC arch/arm/mach-davinci/devices-da8xx.o CC arch/arm/mach-davinci/cp_intc.o CC arch/arm/mach-davinci/board-da850-evm.o CC arch/arm/mach-davinci/cpufreq.o CC arch/arm/mach-davinci/cpuidle.o CC arch/arm/mach-davinci/pm.o AS arch/arm/mach-davinci/sleep.o LD arch/arm/mach-davinci/built-in.o CC kernel/sched.o In file included from include/linux/blkdev.h:12:0, from kernel/sched.c:48: include/linux/pagemap.h: In function 'fault_in_pages_readable': include/linux/pagemap.h:413:16: warning: variable 'c' set but not used [-Wunused-but-set-variable] volatile char c; ^ kernel/sched.c: In function 'alloc_fair_sched_group': kernel/sched.c:9852:13: warning: variable 'rq' set but not used [-Wunused-but-set-variable] struct rq *rq; ^ CC kernel/fork.o In file included from include/linux/mempolicy.h:62:0, from kernel/fork.c:21: include/linux/pagemap.h: In function 'fault_in_pages_readable': include/linux/pagemap.h:413:16: warning: variable 'c' set but not used [-Wunused-but-set-variable] volatile char c; ^ CC kernel/exec_domain.o CC kernel/panic.o CC kernel/printk.o kernel/printk.c: In function 'kmsg_dump': kernel/printk.c:1490:11: warning: variable 'chars' set but not used [-Wunused-but-set-variable] unsigned chars; ^ CC kernel/cpu.o CC kernel/exit.o In file included from include/linux/mempolicy.h:62:0, from kernel/exit.c:31: include/linux/pagemap.h: In function 'fault_in_pages_readable': include/linux/pagemap.h:413:16: warning: variable 'c' set but not used [-Wunused-but-set-variable] volatile char c; ^ CC kernel/itimer.o TIMEC kernel/timeconst.h Can't use 'defined(@array)' (Maybe you should just omit the defined()?) at kernel/timeconst.pl line 373. /home/pfreire/SDKs/DaVinci-PSP-SDK-03.20.00.14/src/kernel/linux-03.20.00.14/kernel/Makefile:133: recipe for target 'kernel/timeconst.h' failed make[1]: *** [kernel/timeconst.h] Error 255 Makefile:885: recipe for target 'kernel' failed make: *** [kernel] Error 2
After copy the new uImage to the microSD card, and started the board, i got this output on minicom:
Welcome to minicom 2.7
OPÇÕES: I18n
Compilado em Feb 7 2016, 13:37:32.
Port /dev/ttyUSB0, 08:23:39
Pressione CTRL-A Z para ajuda sobre teclas especiais
NAND: 512 MiB
MMC: davinci: 0
Bad block table found at page 262080, version 0x01
Bad block table found at page 262016, version 0x01
*** Warning - bad CRC, using default environment
In: serial
Out: serial
Err: serial
ARM Clock : 456000000 Hz
DDR Clock : 150000000 Hz
Net: Ethernet PHY: GENERIC @ 0x07
DaVinci-EMAC
Hit any key to stop autoboot: 0
reading boot.scr
** Unable to read "boot.scr" from mmc 0:1 **
reading uImage
2164968 bytes read
## Booting kernel from Legacy Image at c0700000 ...
Image Name: Linux-2.6.33-rc4
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2164904 Bytes = 2.1 MiB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Anyone can help?
Regards,
Pedro Freire