Hi there,
I am trying to flash an application on the DSP core of the OMAP L138 with the StarterWare boot loader ARM application. When I select targetType as OMAPL138_LCDK all works fine.
When I tried to use OMAPL138 instead of OMAPL138_LCDK as a targetType it get stuck in "Waiting for SFT on OMAP-L138..."
Now I understand the board I am using is OMAPL138_LCDK so that is the right option but would like to understand what is expected when OMAPL138 is selected as the target. Since, it might be useful to change accordingly when we get our prototype boards with OMAPL138 chips. Thanks.
PS: I am using NAND for Flash.
Regards,
Mitesh