Hi Rahul,
Ok that makes sense now... Many thanks.
I have two further questions that you could probably answer very quickly.
1/ is it possible to access the emac using starterware driver (lwIPInit) simultaneously from the ARM (instNum=0) and the DSP (instNum=1) ?
2/ Another issue is that I see that there is a clocking/baud rate issue when using starterware UARTStdioInit() with the omapl128 DSP. Could you point me in the right direction to resolve this? The identical code works fine on the omapl138 ARM.
Best Regards
Andrew