What is the recommended internal trace width connecting to the OMPAPL137? OMAP-L137 traces connect to inline resistors then to buffers.
Internal layer is 0.5oz copper.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the recommended internal trace width connecting to the OMPAPL137? OMAP-L137 traces connect to inline resistors then to buffers.
Internal layer is 0.5oz copper.
Thanks.
Indeed, somehow the links were broken, when I posted. Here they are again:
High-Speed Interface Layout Guidelines:
http://www.ti.com/lit/an/spraar7f/spraar7f.pdf
Starter Kit Design files:
http://support.spectrumdigital.com/boards/evmomapl137/revd/
Best Regards,
Yordan